2.3.19 PHY_ConfigReservedFrameFiltering Function

C

PHY_Retval_t PHY_ConfigReservedFrameFiltering(bool recReservedFrame,
bool bypassFrameFilter )

Summary

Configures TRX for receiving reserved frame

Description

This function is used to configure the trx for receiving the reserved frame type frames and to enable/disable the frame filtering .

Precondition

PHY_Init() should have been called before calling this function.

Parameters

ParamDescription
recReservedFrametrue to enable the reception of reserved frame types acknowledgment after reception
bypassFrameFiltertrue to bypass the frame filtering at the hardware level like data frame as specified in IEEE specification

Returns

PHY_SUCCESS If trx is configured correctly PHY_FAILURE otherwise

Example

PHY_Retval_t retVal = PHY_FAILURE;
bool rxResFrame = true;
bool bypassFrameFiltering = false;

retVal = PHY_ConfigReservedFrameFiltering(rxResFrame, bypassFrameFiltering);
if(PHY_SUCCESS == retVal)
{
    //Trx is configured to receive the reserved frame and to do the frame
    //filtering as stated in IEEE Spec
}

Remarks

None