5.1.1.2 System Design Without Compensation of Initial XTAL and XTO Tolerances
If tuning at the end of module production is not possible, additional tolerances have to be considered and result in broader system bandwidth. The resulting tolerance is given by:
- The internal load capacitance variation and the XTO variation amounts for a motional capacitance of 4 fF in the crystal to ±10 ppm and ±14 ppm. For more details, refer to the ATA8210/ATA8215 UHF ASK/FSK Receiver Data Sheet (9344E), section 4, parameter numbers 13.40 and 13.50.
- The initial frequency tolerance of the crystal of, for example, ±40 ppm
- The temperature tolerance of the crystal, for example, ±30 ppm in the temperature range of -40°C to +85°C(1)
- Crystal aging, for example, ±10 ppm
- Use the RF calibration feature of the ATA8210/15 to reduce the influence of the temperature tolerance.
The total frequency tolerance is ±94 ppm. For a 433.92 MHz system, the total frequency tolerance on one side of the communication system is ±40.78 kHz. If both sides of the system have the same tolerances, a maximum frequency offset between transmitter and receiver of 2 x ±40.78 kHz = ±81.57 kHz has to be taken into account.
Finally, using 10 kBit/s FSK with ±10 kHz frequency deviation results in required IF bandwidth of 191.4 kHz. For the system design, select the IF bandwidth of 219 kHz IF bandwidth. No loss in sensitivity due to frequency offsets has to be considered due to the 27.6 kHz bandwidth margin. For more details on the impact of the IF bandwidth on system performance, see Estimation of Maximum Frequency Offset Between Receiver and Transmitter from Related Links.