5.1.1.3 Estimation of Maximum Frequency Offset Between Receiver and Transmitter
The required channel filter bandwidth depends on the frequency error between the receiver and transmitter and the occupied bandwidth of the modulation signal used. For ASK systems, a frequency transition during the power amplifier switching has to be additionally taken into account if the ATA8710 is used as the ASK transmitter. For more details, see the ASK considerations in the second part of this section.
For more details regarding the main impact of the XTO on the worst case frequency error between the receiver and transmitter, see System Design with Compensation of Initial XTAL and XTO Tolerances from Related Links. The maximum frequency error between the receiver and transmitter has to be determined for the individual application, and the channel filter bandwidth has to be chosen with enough width to prevent the unintentional loss of sensitivity, in the case of worst case frequency errors. The channel bandwidths of the ATA8210/15 can be configured between 25 kHz and 360 kHz. See Channel Filter Bandwidths in the Channel Filter from Related Links.
Channel Filter Bandwidth | Manchester-Coded FSK Data Rate and Frequency Deviation | Measured Frequency Offset ΔfS1.5dBFSK_measured | Calculated Frequency Offset with Equation |
|---|---|---|---|
25 kHz | 0.75 kBit ±0.75 kHz | ±10.7 kHz | ±11.44 kHz |
| 2.4 kBit ±2.4 kHz | ±9.4 kHz | ±9.10 kHz | |
| 5 kBit ±2.4 kHz | ±6.8 kHz | ±6.95 kHz | |
80 kHz | 2.4 kBit ±2.4 kHz | ±35 kHz | ±36.6 kHz |
| 10 kBit ±10 kHz | ±27.5 kHz | ±25.8 kHz | |
| 20 kBit ±20 kHz | ±17.5 kHz | ±11.7 kHz | |
| 165 kHz | 5 kBit ±5 kHz | ±72.5 kHz | ±75.4 kHz |
| 10 kBit ±10 kHz | ±70 kHz | ±68.3 kHz | |
| 20 kBit ±20 kHz | ±57.5 kHz | ±54.2 kHz | |
| 1 kBit ±16 kHz | ±60 kHz | ±66.5 kHz | |
| 10 kBit ±16 kHz | ±70 kHz | ±63.6 kHz | |
366 kHz | 10 kBit ±10 kHz | ±170 kHz | ±168.8 kHz |
| 20 kBit ±20 kHz | ±155 kHz | ±154.7 kHz | |
| 10 kBit ±38 kHz | ±135 kHz | ±143.7 kHz |
The following figure shows the sensitivity loss versus frequency offset for FSK with DR = 2.4 kBit/s and fDEV = ±2.4 kHz using a 80 kHz channel filter bandwidth. The 1.5 dB additional loss in the link budget can be avoided using a slightly higher bandwidth. For more details, see System Design with Compensation of Initial XTAL and XTO Tolerances from Related Links. In the 80 kHz bandwidth, FSK DR = 2.4 kBit/s and fDEV = ±2.4 kHz case using only ±30 kHz maximum frequency offset instead of ±35 kHz avoids the additional 1.5 dB sensitivity loss in the link budget. For the other channel filter bandwidth and data rate examples, the behavior is equivalent. This can be taken into account by lowering the maximum frequency offset by BWIF/16. Equation (53) must be used to incorporate this into the system design. The ripple in the sensitivity in the following figure is caused by ±0.5 dB measurement uncertainty and is not a property of the ATA8210/15.
The following figure shows the sensitivity loss versus frequency offset for DR = 10 kBit/s and fDEV = ±10 kHz using a 165 kHz channel filter bandwidth. The ripple in the sensitivity in the following figure is caused by ±0.5 dB measurement uncertainty and is not a property of the ATA8210/15.
The following table shows the measured and calculated maximum frequency offsets derived from equation (52) for low loss in sensitivity. Microchip recommends using these numbers for system design.
Channel Filter Bandwidth | Manchester Coded FSK Data Rate and Frequency Deviation | Recommended maximum Frequency Offset for Low Loss Based on Measurement | Calculated Frequency Offset with Equation |
|---|---|---|---|
| 25 kHz | 0.75 kBit ±0.75 kHz | ±9.1 kHz | ±9.9 kHz |
| 2.4 kBit ±2.4 kHz | ±7.8 kHz | ±7.5 kHz | |
| 5 kBit ±2.4 kHz | ±5.2 kHz | ±5.4 kHz | |
| 80 kHz | 2.4 kBit ±2.4 kHz | ±30 kHz | ±31.6 kHz |
| 10 kBit ±10 kHz | ±22.5 kHz | ±20.8 kHz | |
| 20 kBit ±20 kHz | ±12.5 kHz | ±6.7 kHz | |
| 165 kHz | 5 kBit ±5 kHz | ±62.2 kHz | ±65.1 kHz |
| 10 kBit ±10 kHz | ±59.7 kHz | ±58 kHz | |
| 20 kBit 20 kHz | ±47.2 kHz | ±43.9 kHz | |
| 1 kBit 16 kHz | ±49.7 kHz | ±56.2 kHz | |
| 10 kBit ±16 kHz | ±59.7 kHz | ±53.3 kHz | |
| 366 kHz | 10 kBit ±10 kHz | ±147 kHz | ±145.9 kHz |
| 20 kBit ±20 kHz | ±132 kHz | ±131.8 kHz | |
| 10 kBit ±38 kHz | ±112 kHz | ±120.8 kHz |
| Channel Filter Bandwidth | Manchester Coded ASK Data Rate | Measured Frequency Offset ΔfS1.5dBASK_measured | Calculated Frequency Offset with Equation (56) |
|---|---|---|---|
| 25 kHz | 2.4 kBit/s | ±11.2 kHz | ±10.1 kHz |
| 5 kBit/s(1) | ±11.2 kHz(1) | ±7.5 kHz | |
| 80 kHz | 2.4 kBit/s | ±37.5 kHz | ±37.6 kHz |
| 10 kBit/s | ±36 kHz | ±30 kHz | |
| 20 kBit/s(1) | ±36 kHz(1) | ±20 kHz | |
| 165 kHz | 2.4 kBit/s | ±77.5 kHz | ±80 kHz |
| 20 kBit/s | ±66 kHz | ±62.5 kHz | |
| 366 kHz | 2.4 kBit/s | ±180 kHz | ±180.6 kHz |
| 20 kBit/s | ±170 kHz | ±163 kHz | |
Note: In the case of high ASK data rates compared
with the bandwidth, the sensitivity versus frequency offset
curve is not as flat as in other cases. For these data rates,
the frequency offset for 3 dB loss of sensitivity is given in
this table and the following table. | |||
The following figure shows the sensitivity versus frequency offset for ASK with DR = 2.4 kBit/s using 165 kHz channel filter bandwidth. The 1.5 dB additional loss in the link budget can also be avoided using the BWIF/16 lower frequency offset, as in the FSK case; therefore, equation (58) must be used for system design.
The preceding figure shows the measured and calculated maximum frequency offset derived from equation (57) for low loss in ASK sensitivity. It is advisable to use this for system design.
| Channel Filter Bandwidth | Manchester Data Rate | Recommended Maximum Frequency Offset for Low Loss Based on Measurement | Calculated Frequency Offset with Equation |
|---|---|---|---|
| 25 kHz | 2.4 kBit/s | ±9.6 kHz | ±8.5 kHz |
| 5 kBit/s(1) | ±9.6 kHz(1) | ±5.9 kHz | |
| 80 kHz | 2.4 kBit/s | ±32.5 kHz | ±32.5 kHz |
| 10 kBit/s | ±31 kHz | ±25 kHz | |
| 20 kBit/s(1) | ±31 kHz(1) | ±15 kHz | |
| 165 kHz | 2.4 kBit/s | ±67 kHz | ±69.5 kHz |
| 20 kBit/s | ±55.5 kHz | ±52.0 kHz | |
| 366 kHz | 2.4 kBit/s | ±157 kHz | ±158 kHz |
| 20 kBit/s | ±147 kHz | ±140 kHz |