6.22.6 clock Function
Determines the processor time used.
Include
<time.h>
Prototype
clock_t clock(void);
Return Value
Returns the number of clock ticks of elapsed processor time.
Remarks
Divide the value returned by this function by the value of the
CLOCKS_PER_SEC macro to determine a time in seconds.
If the target environment cannot measure elapsed processor time, the function returns -1
cast as a clock_t (i.e. (clock_t) -1).
When using XC16 or XC-DSC, this function uses the device Timer2 and Timer3 to compute clock ticks. By default, the compiler returns the time as instruction cycles.
Example
#include <time.h>
#include <stdio.h>
volatile int i;
int main(void)
{
clock_t start, stop;
int ct;
start = clock();
for (i = 0; i < 10; i++)
stop = clock();
printf("start = %ld\n", start);
printf("stop = %ld\n", stop);
}
Example Output
start = 0
stop = 317