6.22.10 localtime Function
Converts a value to the local time.
Include
<time.h>
Prototype
struct tm *localtime(const time_t *tod);
Argument
tod- pointer to stored time
Return Value
Returns the address of the time structure.
Remarks
As time zones are not supported, the localtime() function will return the
same time as gmtime().
By default, both the MPLAB XC16 and XC-DSC compilers returns the time as instruction
cycles. With this default, localtime and gmtime will
be equivalent, except localtime will return tm_isdst
(Daylight Savings Time flag) as -1 to indicate that the status of Daylight Savings Time
is not known.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <time.h>
#include <stdio.h>
int main(void)
{
time_t timer;
struct tm *newtime;
timer = 1066668182; /* Mon Oct 20 16:43:02 2003 */
newtime = localtime(&timer);
printf("Local time = %s\n", asctime(newtime));
}
Example Output
Local time = Mon Oct 20 16:43:02 2003