6.22.9 gmtime Function
Converts calendar time to time structure expressed as Universal Time Coordinated (UTC) also known as Greenwich Mean Time (GMT).
Include
<time.h>
Prototype
struct tm *gmtime(const time_t *tod);
Argument
tod- pointer to stored time
Return Value
Returns the address of the time structure.
Remarks
This function breaks down the tod value into the time
structure of type tm. By default, the compiler returns the time as
instruction cycles. With this default, gmtime and
localtime will be equivalent, except gmtime will
return tm_isdst (Daylight Savings Time flag) as zero to indicate that
Daylight Savings Time is not in effect.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <time.h>
#include <stdio.h>
int main(void)
{
time_t timer;
struct tm *newtime;
timer = 1066668182; /* Mon Oct 20 16:43:02 2003 */
newtime = gmtime(&timer);
printf("UTC time = %s\n", asctime(newtime));
}
Example Output
UTC time = Mon Oct 20 16:43:02 2003