6.22.13 time Function
Calculates the current calendar time.
Include
<time.h>
Prototype
time_t time(time_t * tod);
Argument
tod- pointer to storage location for time
Return Value
Returns the calendar time encoded as a value of time_t.
Remarks
If the pointer argument is not NULL, the time value is written to the
address held by this pointer.
If the target environment cannot determine the time, the function returns -1 cast as a
time_t. By default, the compiler returns the time as instruction
cycles.
When using MPLAB XC16 or XC-DSC, this function uses the device Timer2 and Timer3 to compute the current time.
When using MPLAB XC8 for AVR devices, this function returns 0 by default. User code can
call set_system_time() at program startup to initialize the system
clock, can call system_tick() to increment the clock (typically
performed using a timer interrupt), and then call time() to obtain the
time value. See the avr/avr/include/sys/time.h source file for
further information.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <time.h>
#include <stdio.h>
volatile int i;
int main(void)
{
time_t ticks;
time(0); /* start time */
for (i = 0; i < 10; i++) /* waste time */
continue;
time(&ticks); /* get time */
printf("Time = %ld\n", ticks);
}
Example Output
Time = 256