6.22.11 mktime Function
Converts local time to a calendar value.
Include
<time.h>
Prototype
time_t mktime(struct tm *tptr);
Argument
tptr- a pointer to the time structure
Return Value
Returns the calendar time encoded as a value of time_t.
Remarks
If the calendar time cannot be represented, the function returns -1 cast as a
time_t (i.e. (time_t) -1).
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <time.h>
#include <stdio.h>
int main(void)
{
time_t timer, whattime;
struct tm *newtime;
timer = 1066668182; /* Mon Oct 20 16:43:02 2003 */
/* localtime allocates space for struct tm */
newtime = localtime(&timer);
printf("Local time = %s", asctime(newtime));
whattime = mktime(newtime);
printf("Calendar time as time_t = %ld\n",
whattime);
}
Example Output
Local time = Mon Oct 20 16:43:02 2003
Calendar time as time_t = 1066668182