10.6.1 Starting from Reset
The internal reset is immediately asserted when a reset source goes active. The
internal reset is kept asserted until the reset source is released and the start-up
sequence is completed. The start-up sequence includes three steps, as follows.
- The first step after the reset
source has been released consists of the device counting the reset start-up
time. The purpose of this reset start-up time is to ensure that supply voltage
has reached sufficient levels. The reset start-up time is counted using the
internal 128kHz oscillator. Note: The actual supply voltage is not monitored by the start-up logic. The device will count until the reset start-up time has elapsed even if the device has reached sufficient supply voltage levels earlier.
- The second step is to count the oscillator start-up time, which ensures that the calibrated internal oscillator has reached a stable state before it is used by the other parts of the system. The calibrated internal oscillator needs to oscillate for a minimum number of cycles before it can be considered stable.
- The last step before releasing the internal reset is to load the calibration and the configuration values from the Non-Volatile Memory to configure the device properly. The configuration time is listed in the next table.
There are two start-up time options which will be supported :
- Normal start-up time: 64ms
- Fast start-up time: 8ms
| Reset | Oscillator | Configuration | Total start-up time |
|---|---|---|---|
| 64ms | 6cycles | 21cycles | 64ms + 6 oscillator cycles + 21 system clock cycles (1) |
| Reset | Oscillator | Configuration | Total start-up time |
|---|---|---|---|
| 8ms | 6cycles | 21cycles | 8 ms + 6 oscillator cycles + 21 system clock cycles (1) |
Note:
- After powering up the device or after a reset the system clock is automatically set to calibrated internal 8MHz oscillator, divided by 8