These bits define the division factor between the selected clock
source and the internal system clock. These bits can be written run-time to vary
the clock frequency to suit the application requirements. As the divider divides
the master clock input to the MCU, the speed of all synchronous peripherals is
reduced when a division factor is used. The division factors are given in the
table below.
Table 10-6. Clock Prescaler Select| CLKPS[3:0] | Clock Division Factor |
|---|
| 0000 | 1 |
| 0001 | 2 |
| 0010 | 4 |
| 0011 | 8 (default) |
| 0100 | 16 |
| 0101 | 32 |
| 0110 | 64 |
| 0111 | 128 |
| 1000 | 256 |
| 1001 | Reserved |
| 1010 | Reserved |
| 1011 | Reserved |
| 1100 | Reserved |
| 1101 | Reserved |
| 1110 | Reserved |
| 1111 | Reserved |
To avoid unintentional changes of clock frequency, a protected change sequence
must be followed to change the CLKPS bits:
- Write the signature for change enable of protected I/O register to
register CCP
- Within four instruction cycles, write the desired value to CLKPS bits
At start-up, CLKPS bits are reset to 0b0011 to select the clock division factor
of 8. If the selected clock source has a frequency higher than the maximum
allowed the application software must make sure a sufficient division factor is
used. To make sure the write procedure is not interrupted, interrupts must be
disabled when changing prescaler settings.