6.4.6 FFTComplexIP
Description
FFTComplexIP computes the Fast Fourier Transform of a source complex vector in place.
Prototype
fractcomplex* FFTComplexIP (int log2N, fractcomplex* srcCV, fractcomplex* twidFactors);
Arguments
|
Parameters |
Description |
|---|---|
|
log2N |
Base 2 logarithm of N (number of complex elements in source vector) |
|
srcCV |
Pointer to the source vector |
|
twidFactors |
Pointer to twiddle factors |
Return
Pointer to the base address of the destination sample.
Remarks
N must be an integer power of 2.
The elements in the source complex vector are expected in a natural order. The resulting transform is stored in bit-reverse order.
The srcCV vector must be allocated in the Y-Data space with address alignment to a modulo of N.
To avoid saturation (overflow) during computation, the values of the source vector should be in the range [-0.5, 0.5].
Only the first N/2 twiddle factors are needed.
The twiddle factors must be initialized with conjFlag set to zero.
Output is scaled by the factor of N.
Source File
- fft_aa.s
Function Profile
|
Program Words |
PIC32A |
|
46 |
|
Cycle count |
Transform Size (N) |
PIC32A | |
|
Cycles if Twiddle Factors in X-mem |
Cycles if Twiddle Factors in P-mem | ||
|
32 |
1,780 |
2,318 | |
|
64 |
4,060 |
5,356 | |
|
128 |
9,188 |
12,228 | |
|
256 |
20,588 |
27,564 | |
|
512 |
45,684 |
61,428 | |
|
1024 |
100,476 |
135,548 | |
|
2048 |
219,268 |
296,580 | |
System resource usage
- W0…W7 - used, not restored
- W8…W14 - saved, used, restored
- ACCA/ACCB - used, not restored
- CORCON - saved, used, restored
- REPEAT instruction(s) usage – 1