6.4.5 FFTComplex
Description
FFTComplex computes the Fast Fourier Transform of a source complex vector and stores the results in the destination complex vector.
Prototype
fractcomplex* FFTComplex(int log2N, fractcomplex* dstCV, fractcomplex* srcCV, fractcomplex* twidFactors);
Arguments
|
Parameters |
Description |
|---|---|
|
log2N |
Base 2 logarithm of N (number of complex elements in source vector) |
|
dstCV |
Pointer to the destination vector |
|
srcCV |
Pointer to the source vector |
|
twidFactors |
Pointer to twiddle factors |
Return
Pointer to the base address of the destination sample.
Remarks
N must be an integer power of 2.
This function internally calls VectorCopy, FFTComplexIP and BitReversal functions.
This function operates out of place. A complex vector, large enough to receive the results of the operation, must already have been allocated and assigned to dstCV.
The elements in the source complex vector are expected in a natural order, and the resulting transform in the destination vector is stored back in a natural order.
The dstCV vector must be allocated in the Y-Data space with address alignment to a modulo of N.
To avoid saturation (overflow) during computation, the values of the source vector should be in the range [-0.5, 0.5].
Only the first N/2 twiddle factors are needed.
The twiddle factors must be initialized with the conjFlag set to zero.
The output is scaled by the factor of N.
Source File
- fftoop_aa.s
Function Profile
|
Program Words |
9 |
|
Cycle Count |
36 |
- The above-mentioned program word and cycle counts pertain solely to FFTComplex. However, as this function inherently utilizes VectorCopy, FFTComplexIP and BitReversalComplex, the respective counts for these functions must also be considered.
- In the description of VectorCopy, FFTComplexIP and BitReversalComplex, the number of cycles reported includes four cycles of C-function call overhead. Thus, the number of actual cycles from these function to add to FFTComplex is 3x4 less than whatever number is reported for a stand-alone FFTComplex.
System resource usage
The below system resource usages exclude that of VectorCopy, FFTComplexIP and BitReversalComplex.
- W0…W4 - used, not restored
- REPEAT instruction usage - None