6.4.3 DCT
Description
DCT computes the Discrete Cosine Transform of a source vector.
Prototype
fractcomplex* DCT (int log2N, fractional* dstCV, fractcomplex* srcCV, fractcomplex* cosFactors, fractcomplex* twidFactors);
Arguments
|
Parameters |
Description |
|---|---|
|
log2N |
Base 2 logarithm of N (number of complex elements in source vector) |
|
dstCV |
Pointer to the destination vector |
|
srcCV |
Pointer to the source vector |
|
cosFactors |
Pointer to the cosine factors |
|
twidFactors |
Pointer to the twiddle factors |
Return
Pointer to the base address of the destination sample.
Remarks
This function internally uses DCTIP and the VectorZeroPad function.
N must be an integer power of 2.
A vector of size 2N elements must already have been allocated and assigned to dstCV.
The dstCV vector must be allocated in the Y-Data space with address alignment to a modulo of N.
The results of the computation are stored in the first N elements of destination vector.
To avoid saturation (overflow) during computation, the values of the source vector should be in the range [-0.5, 0.5].
Only the first N/2 cosine factors are needed.
Only the first N/2 twiddle factors are needed.
The twiddle factors must be initialized with conjFlag set to a value different than zero.
Output is scaled by the factor of N.
Source File
- dctoop_aa.s
Function Profile
|
Program Words |
64 |
|
Cycle Count |
33 |
- The above-mentioned program word and cycle counts pertains solely to DCT. However, as this function inherently utilizes DCTIP and VectorZeroPad, the respective counts for DCTIP and VectorZeroPad must also be considered.
- In the description of DCTIP and VectorZeroPad, the number of cycles reported includes four cycles of C-function call overhead. Thus, the number of actual cycles from DCTIP and VectorZeroPad to add to DCT is 2x4 less than whatever number is reported for a stand-alone DCTIP/VectorZeroPad.
System resource usage
The below system resource usages exclude that of DCTIP and VectorZeroPad.
- W0…W5 - used, not restored
- REPEAT instruction usage - None