5.5.13 IIRLattice
Description
IIRLattice uses a lattice structure implementation to apply an IIR filter to the sequence of the source samples. It then places the results in the sequence of the destination samples and updates the delay values.
Prototype
typedef struct {
int order;
fractional* kappaVals;
fractional* gammaVals;
fractional* delay;
} IIRLatticeStruct;fractional* IIRLattice (int numSamps, fractional* dstSamps, fractional* srcSamps, IIRLatticeStruct* filter);
Arguments
Filter Structure:
|
Parameters |
Description |
|---|---|
|
order |
Filter order (also M, M ≤ N; see FIRLattice for N) |
|
kappaVals |
Base address for lattice coefficients (also k), either in X-Data or program memory |
|
gammaVals |
Base address for ladder coefficients (also g), either in X-Data or program memory. If NULL, the function will implement an all-pole filter. |
|
delay |
Base address for delay (also d), only in Y-Data |
Filter Description:
| Parameters |
Description |
|---|---|
|
numSamps |
Number of input samples to filter (also N; with N being multiple of R) |
|
dstSamps |
Pointer to the destination samples (also y) |
|
srcSamps |
Pointer to the source samples (also x) |
|
filter |
Pointer to the IIRLatticeStruct filter structure |
Return
Pointer to the base address of the destination sample.
Remarks
Lattice coefficients, k[m], defined in 0 ≤ m ≤ M.
Ladder coefficients, g[m], defined in 0 ≤ m ≤ M (unless if implementing an all-pole filter).
Delay, d[m], defined in 0 ≤ m ≤ M.
Source samples, x[n], defined in 0 ≤ n < N.
Destination samples, y[n], defined in 0 ≤ n < N.
Appropriately scaling the input signal, prior to applying the filter, should prevent the fractional implementation from saturating.
Source File
- iirlatt_aa.s
Cycle counts for PIC32A:
| Source Vector Size | Cycles if coefficients in X-mem | Cycles if coefficients in P-mem |
|---|---|---|
|
32 |
9586 |
15290 |
|
64 |
19122 |
30522 |
|
128 |
38194 |
60986 |
|
256 |
76338 |
121914 |
|
512 |
152626 |
243770 |
|
1024 |
305202 |
487482 |
|
2048 |
610254 |
774906 |
(*All values with M = 32)
System resource usage
- W0…W7 - used, not restored
- W8…W14 - saved, used, restored
- ACCA - used, not restored
- CORCON - saved, used, restored
- REPEAT instruction(s) usage – None