2 Programming the Device on the Evaluation Kit
(Ask a Question)Once the design is created through TCL scripts as mentioned in Appendix 4: Running the TCL Script, open the design in Libero® SoC software. To program the PolarFire® device, perform the following steps:
- Ensure that the jumper settings on the board are same as listed in the following table.
Table 2-1. Jumper Settings on Evaluation Kit Jumper Description J18, J19, J20, J21, and J22 Close pin 2 and 3 for programming the PolarFire FPGA through FTDI J28 Close pin 1 and 2 for programming through the on-board FlashPro5 J26 Close pin 1 and 2 for programming through the FTDI SPI J27 Close pin 1 and 2 for programming through the FTDI SPI J4 Close pin 1 and 2 for manual power switching using SW3 J12 Close pin 3 and 4 for 2.5V J46 Close pin 1 and 2 for routing 125 MHz differential clock oscillator output to the line side. Open pin 1 and 2 for routing 122.88 MHz differential clock oscillator output to the line side.
- Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the Host PC to J5 (FTDI port) on the board.
- Power on the board using the SW3 slide switch.
- Connect TXN to RXN and TXP to RXP using the two SMA to SMA cables, see the following figure. The following figure shows the board setup.
Figure 2-1. Board Setup for Evaluation Kit - Double-click Run PROGRAM Action.
When the device is programmed successfully, a green tick mark appears, see the following figure. See Running the Demo to run the multi-rate transceiver demo.