9 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the current publication.

Table 9-1. Revision History
RevisionDateDescription
B03/2025The following is the summary of the changes made in B revision.
A08/2022The following is the summary of the changes made in A revision.
  • The document was migrated to the Microchip template.
  • The document number was updated to DS00004662A from 50200759.
  • The document ID was updated to AN4662 from DG0759.
  • Removed Splash Kit content throughout the document.
  • Updated figures in Figure 1-1.
  • Updated Design Implementation figures throughout the document.
  • Updated content of Simulating Design section throughout the document.
  • Updated Simulation Flow figures throughout the document.
  • Updated Figure 1-1, Figure 1-6, Figure 1-11, Figure 1-16, and Figure 5-1.
  • Updated all table of Resource Utilization section.
  • Updated all figures of Running the Demo.
  • Updated all figures of How to Use SmartBERT.
  • Updated all design file locations throughout the document.
  • Updated all figures of Appendix 3: Programming the Device Using FlashPro Express.
10.0—The following is a summary of the changes made in this revision.
  • Updated the document for Libero SoC v12.2.
  • Removed the references to Libero version numbers.
9.0—The document was updated for Libero SoC v12.0.
8.0—Merged Splash kit related content and updated the document for Libero SoC PolarFire v2.3.
7.0—The document was updated for Libero SoC PolarFire v2.2.
6.0—The document was updated for Libero SoC PolarFire v2.1.
5.0—The following is a summary of the changes made in revision 5.0 of this document.
  • The document was updated to include features and enhancements introduced in the Libero® SoC PolarFire® v2.0 release.
  • Information about the usage of the SmartBert IP was added. See Appendix 2: How to Use SmartBert IP.
4.0—The design files were updated to include enhancements to the GUI logic.
3.0—The following is a summary of the changes made in revision 3.0 of this document.
  • The document was updated to include features and enhancements introduced in the Libero® SoC PolarFire® v1.1 SP1 release.
  • Information about programming the device and running the demo was added. See Programming the Device Using FlashPro and Running the Demo.
  • A list of reference documents was added. See Appendix 4: References.
2.0—Revision 2.0 of this document included the demonstration of PolarFire transceivers used in 64b66b mode. See Reference Design 3: 64b66b Design, page 15.
1.0—The first publication of this document.