7 Appendix 4: Running the TCL Script
(Ask a Question)TCL scripts are provided in the design files folder under directory mpf_an4662_df/HW/<8b10b/64b66b/PMA/PMA_bitslip/Smartbert>. If required, the design flow can be reproduced from Design Implementation till the generation of job file.
To run the TCL, perform the following steps:
- Launch the Libero software.
- Select
- Click Browse and select
script.tclfrom the downloadedHWdirectory. - Click Run.
After successful execution of TCL script, Libero project is created within HW directory. For more information about TCL scripts, see mpf_an4662_df/TCL_Script_readme.txt.
For more details on TCL commands, see Tcl Commands Reference Guide . Contact Technical Support for any queries encountered while running the TCL script.
Important: While running the scripts, simulation runs in the Batch mode by default, which takes more time for the design to complete the build and compilation. If you do not want to run simulation, then you can comment the simulation flow command in the
script.tcl.