28.2.29 __builtin_fma
Description
__builtin_fma computes (x * y) + z as if with unlimited
range and precision, rounding only once to the result format. This can provide more
accurate results than performing the multiplication and addition separately, especially
with floating-point numbers. This function operates on 64-bit, double-precision
floating-point numbers. For more information, see 9.3 Floating-Point Data Types.
Prototype
double __builtin_fma(double x, double y, double z);
Arguments
x - value to be multiplied by the multiplier
y - value of multiplier
z - value to added to the result of the
multiplication
Return Value
Returns value of the mathematical and rounding operations. See also 4.3.4.1 Why Are My Floating-Point Results Not Quite What I Am Expecting?
Machine Instruction
mac.d
Error Messages
An error message is reported if there is a floating-point exception.