28.2.82 __builtin_write_DISICTL
Description
Disable interrupts at or below the threshold given by the argument (an argument of zero
will enable all interrupts). The current interrupt priority threshold is returned; the
return result may be omitted by casting the expression to void .
Prototype
uint32_t __builtin_write_DISICTL(uint32_t threshold);
Argument
threshold - new interrupt priority threshold
Return Value
Return the previous interrupt priority threshold.
Machine Instruction
disictl
Error Messages
If a literal value is provided, it must within the range of 0 to 7; a compile time error
message will be reported the threshold argument is
outside of these bounds.