1.3.5.1.6 PRIME_API_Tasks Function
C
void PRIME_API_Tasks(void)
Summary
Maintains PRIME Library State Machine.
Description
This function is used to maintain the PRIME Library internal state machine and generate callbacks.
Precondition
The PRIME_API_Initialize function should have been called before calling this function.
Parameters
None.
Returns
None.
Example
while (true)
{
PRIME_API_Tasks();
}
Remarks
This routine is normally not called directly by an application. The PRIME application must use the function located in the PRIME API and call it periodically.