1.5.5.4.24 SRV_FU_RegisterCallbackCrc Function

C

void SRV_FU_RegisterCallbackCrc(SRV_FU_CRC_CB callback);

Summary

Registers a function to be called back when the CRC of the received image has been calculated.

Description

This function allows the PRIME stack to register a function to be called back when the CRC of the received image has been calculated.

Parameters

ParametersDescription
callbackPointer to the callback function

Returns

None.

Example

    void _check_crc(uint32_t crc)
    {
        ...
    }

    void main(void)
    {
        SRV_FU_Initialize();

        SRV_FU_RegisterCallbackCrc(_check_crc);
    }
    

Remarks

This function is called by the PRIME stack.