1.5.5.4.21 SRV_FU_RegisterCallbackMemTransfer Function

C

void SRV_FU_RegisterCallbackMemTransfer(SRV_FU_MEM_TRANSFER_CB callback);

Summary

Registers a function to be called back when a memory operation finishes.

Description

This function allows the PRIME stack to register a function to be called back when a memory operation finishes.

Parameters

ParametersDescription
callbackPointer to the callback function

Returns

None.

Example

    void _endMemoryTransaction(SRV_FU_MEM_TRANSFER_CMD command,
                   SRV_FU_MEM_TRANSFER_RESULT result)
    {
        ...
    }

    void main(void)
    {
        SRV_FU_Initialize();

        SRV_FU_RegisterCallbackMemTransfer(_endMemoryTransaction);
    }

Remarks

This function is called by the PRIME stack.