1.5.5.4.18 SRV_FU_SetECDSAPublicKey Function

C

void SRV_FU_SetECDSAPublicKey(uint8_t *pubKey, uint32_t pubKeyLen);

Summary

Set the Firmware Upgrade the public key to be used for the ECDSA-256 signature.

Description

This function sets the public key to be used for the ECDSA-256 signature.

Parameters

ParametersDescription
pubKeyPointer to the buffer where the ECDSA-256 public key is stored
pubKeyLenLength of the key

Returns

None.

Example

    #define LEN_PUBLIC_KEY 65

    uint8_t pubKey[LEN_PUBLIC_KEY];
    uint16_t pubKeyLen = LEN_PUBLIC_KEY;

    SRV_FU_SetECDSAPublicKey(pubKey, pubKeyLen);

Remarks

This function is called by the application.