1.5.5.4.26 SRV_FU_RegisterCallbackVerify Function

C

void SRV_FU_RegisterCallbackVerify(SRV_FU_IMAGE_VERIFY_CB callback);

Summary

Registers a function to be called back when the received image has been verified.

Description

This routine allows the PRIME stack to register a function to be called back when the received image has been verified.

Parameters

ParametersDescription
callbackPointer to the callback function

Returns

None.

Example

    void _image_verification(SRV_FU_VERIFY_RESULT verifyResult)
    {
        ...
    }

    void main(void)
    {
        SRV_FU_Initialize();

        SRV_FU_RegisterCallbackVerify(_image_verification);
    }
    

Remarks

This function is called by the PRIME stack.