1.4.3.25 PAL_GetCD Function

C

uint8_t PAL_GetCD(uint16_t pch, uint8_t *cd, uint8_t *rssi, uint32_t *timeVal,
    uint8_t *header);

Summary

Get the carrier detect signal.

Description

This routine is used to get the value of carrier detect signal.

Precondition

The PAL_Initialize function should have been called before calling this function.

Parameters

ParametersDescription
pchPhysical channel
cdCarrier detect signal output parameter
rssiReceived signal strength indicator
timeValCurrent time in µs
headerHeader type

Returns

  • PAL_CFG_SUCCESS: If successful
  • PAL_CFG_INVALID_INPUT: If unsuccessful

Example

    uint8_t result=PAL_CFG_SUCCESS;
    uint8_t cd=0;
    uint8_t rssi=0;
    uint32_t timeVal=0;
    uint8_t header=0;
    uint16_t pch=1;

    result = PAL_GetCD(pch, &cd, &rssi, &timeVal, &header);

Remarks

Not available for both PHY Serial and PHY RF.