1.4.3.32 PAL_ProgramChannelSwitch Function
C
void PAL_ProgramChannelSwitch(uint32_t timeSync, uint16_t pch,
uint8_t timeMode);
Summary
Program a pch switch in the given time.
Description
This routine is used to program a pch switch in the given time.
Precondition
The PAL_Initialize function should have been called before calling this function.
Parameters
| Parameters | Description |
|---|---|
| timeSync | Initial pch switch time in µs |
| pch | Physical Channel to be updated |
| timeMode | Channel Switch Time mode |
Returns
None.
Example
uint32_t timeSync = 10000 uint16_t pch = 600; uint8_t timeMode = PAL_TX_MODE_ABSOLUTE; PAL_ProgramChannelSwitch(timeSync, pch, timeMode);
Remarks
Only available for PHY RF.