1.4.3.31 PAL_SetChannel Function

C

uint8_t PAL_SetChannel(uint16_t pch);

Summary

Set the band (PLC) or the pch (RF).

Description

This routine is used to set the pch or band used for the communication.

Precondition

The PAL_Initialize function should have been called before calling this function.

Parameters

ParametersDescription
pchPhysical channel

Returns

  • PAL_CFG_SUCCESS: If successful
  • PAL_CFG_INVALID_INPUT: If unsuccessful

Example

    uint8_t result=PAL_CFG_SUCCESS;
    uint16_t pch=1;

    result = PAL_SetChannel(pch);

Remarks

Not available for PHY Serial.