1.4.3.26 PAL_GetNL Function

C

uint8_t PAL_GetNL(uint16_t pch, uint8_t *noise);

Summary

Get the noise floor level value.

Description

This routine is used to know the noise level present in the power line.

Precondition

The PAL_Initialize function should have been called before calling this function.

Parameters

ParametersDescription
pchPhysical channel
noiseNoise floor level output parameter

Returns

  • PAL_CFG_SUCCESS: If successful
  • PAL_CFG_INVALID_INPUT: If unsuccessful

Example

    uint8_t result=PAL_CFG_SUCCESS;
    uint8_t nl=0;
    uint16_t pch=1;

    result = PAL_GetNL(pch, &nl);

Remarks

Not available for PHY Serial.