1.4.3.29 PAL_GetCCA Function

C

uint8_t PAL_GetCCA(uint16_t pch, uint8_t *pState);

Summary

Get clear pch assessment mode value.

Description

This routine is used to get the clear pch assesment mode. The pch state helps to know whether or not the RF physical medium is free.

Precondition

The PAL_Initialize function should have been called before calling this function.

Parameters

ParametersDescription
pchPhysical channel
pStateChannel state (0: busy, 1: free) of RF module

Returns

  • PAL_CFG_SUCCESS: If successful
  • PAL_CFG_INVALID_INPUT: If unsuccessful

Example

    uint8_t result=PAL_CFG_SUCCESS;
    uint8_t pState=0;
    uint16 pch = 512;

    result = PAL_GetCCA(pch, &pState);

Remarks

Only implemented in PHY RF interface.