8.2 Page Write
A page write sequence allows up to 128 bytes to be written in the same write cycle, provided that all bytes are in the
same row of the memory array. Partial page writes of less than 128 bytes are allowed. After each byte of data is received, the seven lowest order address bits are internally
incremented following the receipt of each data byte. The higher order address bits are not
incremented and retain the memory array page location. If more bytes of data are
transmitted that what will fit to the end of that memory row, the address counter will
rollover to the beginning of the same row. Nevertheless, creating a rollover event should
be avoided as previously loaded data in the page could become unintentionally altered. The
AT25512 is automatically returned to the Write
Disable state (WEL = 0) at the completion of a write cycle.
- This instruction initiates a self‑timed internal write cycle (tWC) on the rising edge of CS after a valid sequence.