5.2.9.13 ZGP_Status_t Enumeration
Syntax
typedef enum
{
ZGP_SUCCESS_STATUS = 0x00,
/** ZGP Data request queue is full */
ZGP_TX_QUEUE_FULL = 0x70,
/* previous GPDF is overwritten */
ZGP_ENTRY_REPLACED = 0x71,
/* GPDF is added to the zgp TxQueue */
ZGP_ENTRY_ADDED = 0x72,
/* zgpTxQueueEntryLifetime timeout */
ZGP_ENTRY_EXPIRED = 0x73,
ZGP_ENTRY_REMOVED = 0x74,
ZGP_GPDF_SENDING_FINALIZED = 0x75,
/* No reply received for commissioning request */
ZGP_NO_COMMISSIONING_REPLY = 0x76,
/* No confirmation for commissioning request */
ZGP_COMMISSIONING_TIMEOUT = 0x77,
/* Commissioning reply has invalid parameter */
ZGP_COMMISSIONING_REPLY_FAILURE = 0x78,
/* Commissioning/Decommissioning invalid request */
ZGP_COMMISSIONING_REQ_INVALID = 0x79,
/* ZGP key unavailable*/
ZGP_UNAVAILABLE_KEY_STATUS = 0x7A,
/* ZGP bad state */
ZGP_BAD_STATE = 0x7B,
/* Invalid parameter */
ZGP_INVALID_PARAMETER = 0x7C,
/* Invalid parameter */
ZGP_NO_CHANNEL_MASK = 0x7D,
/* ZGP_SECURITY_LEVEL_NOT_MATCHED */
ZGP_SECURITY_LEVEL_NOT_MATCHED = 0x7E,
/* No reply received for channel request*/
ZGP_NO_CHANNEL_CONFIG_REPLY = 0x7F,
/** IEEE 802.15.4-2006, Table 78 MAC enumerations description. */
/** The frame counter purportedly applied by the originator of the
* received frame is invalid. */
ZGP_MAC_COUNTER_ERROR_STATUS = 0xDB,
/** The key purportedly applied by the originator of the received frame is
* not allowed to be used with that frame type according to the key usage
* policy of the recipient. */
ZGP_MAC_IMPROPER_KEY_TYPE_STATUS = 0xDC,
/** The security level purportedly applied by the originator of the received
* frame does not meet the minimum security level required/expected by
* the recipient for that frame type. */
ZGP_MAC_IMPROPER_SECURITY_LEVEL_STATUS = 0xDD,
/** The received frame was purportedly secured using security based on
* IEEE Std 802.15.4-2003, and such security is not supported by this standard.
**/
ZGP_MAC_UNSUPPORTED_LEGACY_STATUS = 0xDE,
/** The security purportedly applied by the originator of the received frame
* is not supported. */
ZGP_MAC_UNSUPPORTED_SECURITY_STATUS = 0xDF,
/** The beacon was lost following a synchronization request. */
ZGP_MAC_BEACON_LOSS_STATUS = 0xE0,
/** A transmission could not take place due to activity on the channel,
* i.e., the CSMA-CA mechanism has failed. */
ZGP_MAC_CHANNEL_ACCESS_FAILURE_STATUS = 0xE1,
/** The GTS request has been denied by the PAN coordinator. */
ZGP_MAC_DENIED_STATUS = 0xE2,
/** The attempt to disable the transceiver has failed. */
ZGP_MAC_DISABLE_TRX_FAILURE_STATUS = 0xE3,
/** Either a frame resulting from processing has a length that is
* greater than aMaxPHYPacketSize or a requested transaction is
* too large to fit in the CAP or GTS. */
ZGP_MAC_FRAME_TOO_LONG_STATUS = 0xE5,
/** The requested GTS transmission failed because the specified
* GTS either did not have a transmit GTS direction or was not defined. */
ZGP_MAC_INVALID_GTS_STATUS = 0xE6,
/** A request to purge an MSDU from the transaction queue was made using
* an MSDU handle that was not found in the transaction table. */
ZGP_MAC_INVALID_HANDLE_STATUS = 0xE7,
/** A parameter in the primitive is either not supported or is out of
* the valid range. */
ZGP_MAC_INVALID_PARAMETER_STATUS = 0xE8,
/** No acknowledgment was received after macMaxFrameRetries. */
ZGP_MAC_NO_ACK_STATUS = 0xE9,
/** A scan operation failed to find any network beacons. */
ZGP_MAC_NO_BEACON_STATUS = 0xEA,
/** No response data were available following a request. */
ZGP_MAC_NO_DATA_STATUS = 0xEB,
/** The operation failed because a 16-bit short address was not allocated. */
ZGP_MAC_NO_SHORT_ADDRESS_STATUS = 0xEC,
/** A receiver enable request was unsuccessful because it could not be
* completed within the CAP. */
ZGP_MAC_OUT_OF_CAP_STATUS = 0xED,
/** A PAN identifier conflict has been detected and communicated
* to the PAN coordinator. */
ZGP_MAC_PAN_ID_CONFLICT_STATUS = 0xEE,
/** A coordinator realignment command has been received. */
ZGP_MAC_REALIGNMENT_STATUS = 0xEF,
/** The transaction has expired and its information was discarded. */
ZGP_MAC_TRANSACTION_EXPIRED_STATUS = 0xF0,
/** There is no capacity to store the transaction. */
ZGP_MAC_TRANSACTION_OVERFLOW_STATUS = 0xF1,
/** The transceiver was in the transmitter enabled state when the receiver
* was requested to be enabled. */
ZGP_MAC_TX_ACTIVE_STATUS = 0xF2,
/** The key purportedly used by the originator of the received frame is
* not available or, if available, the originating device is not known
* or is blacklisted with that particular key. */
ZGP_MAC_UNAVAILABLE_KEY_STATUS = 0xF3,
/** A SET/GET request was issued with the identifier of a PIB
* attribute that is not supported. */
ZGP_MAC_UNSUPPORTED_ATTRIBUTE_STATUS = 0xF4,
/** A request to send data was unsuccessful because neither the source address
* parameters nor the destination address parameters were present. */
ZGP_MAC_INVALID_ADDRESS_STATUS = 0xF5,
/** A receiver enable request was unsuccessful because it specified a number
* of symbols that was longer than the beacon interval. */
ZGP_MAC_ON_TIME_TOO_LONG_STATUS = 0xF6,
/** A receiver enable request was unsuccessful because it could not be
* completed within the current superframe and was not permitted to be
* deferred until the next superframe. */
ZGP_MAC_PAST_TIME_STATUS = 0xF7,
/** The device was instructed to start sending beacons based on the
* timing of the beacon transmissions of its coordinator, but the device
* is not currently tracking the beacon of its coordinator. */
ZGP_MAC_TRACKING_OFF_STATUS = 0xF8,
/** An attempt to write to a MAC PIB attribute that is in a table failed
* because the specified table index was out of range. */
ZGP_MAC_INVALID_INDEX_STATUS = 0xF9,
/** There are some unscanned channels yet, but there is no memory */
ZGP_MAC_LIMIT_REACHED_STATUS = 0xFA,
/** A SET/GET request was issued with the identifier of an attribute
* that is read only. */
ZGP_MAC_READ_ONLY_STATUS = 0xFB,
/** A request to perform a scan operation failed because the MLME was
* in the process of performing a previously initiated scan operation. */
ZGP_MAC_SCAN_IN_PROGRESS_STATUS = 0xFC,
/** The device was instructed to start sending beacons based on the timing of
* the beacon transmissions of its coordinator, but the instructed start time
* overlapped the transmission time of the beacon of its coordinator. */
ZGP_MAC_SUPERFRAME_OVERLAP_STATUS = 0xFD
}ZGP_Status_t;Description
The ZGP_Status_t enumeration represents the return codes for ZGP
primitives, indicating the success or failure of an operation.