7.2.1 Configuration Settings
(Ask a Question)The following table lists the description of the configuration parameters used in the hardware implementation of T-Format Interface. These are generic parameters and are varied as per the requirement of the application.
| Signal Name | Description |
|---|---|
| g_TIMEOUT_TIME | Defines the timeout time between successive fields in a frame in multiples of sys_clk_i period. |
| g_FAULT_THRESHOLD | Defines the fault threshold value – alarm_o is asserted when the fault counter exceeds this value. |