16.4.1 Simulation
(Ask a Question)The following steps describe how to simulate the core using the testbench:
- Go to Libero SoC Catalog
tab, expand Solutions-MotorControl, double click Stepper
Theta Generation, and then click OK. The
documentation associated with the IP are listed under
Documentation. Important: If you do not see the Catalog tab, navigate to menu and click Catalog to make it visible.
Figure 16-8. Stepper Theta Generation IP Core in Libero SoC Catalog - On the Stimulus Hierarchy
tab, select the testbench (
stepper_theta_tb.v), right click and then click .Important: If you do not see the Stimulus Hierarchy tab, navigate to menu and click Stimulus Hierarchy to make it visible.Figure 16-9. Simulating Pre-Synthesis Design ModelSim opens with the testbench file, as shown in the following figure.
Figure 16-10. ModelSim Simulation Window
Important: If the simulation is interrupted due to the
runtime limit specified in the
.do file, use the run
-all command to complete the simulation.