1.2.1.1.1.12 AES counter-measures mask load
CMMASK_API_FILE Macro
C
#define CMMASK_API_FILE
@file @copyright Copyright (c) 2019-2020 Silex Insight. All Rights reserved.
Examples: The following example shows typical sequence of function calls for loading the counter-measure mask. @code SX_CM_LOAD_MASK(ctx, value) SX_CM_LOAD_MASK_WAIT(ctx) @endcode
Loads random used in the AES counter-measures.
SX_CM_LOAD_MASK Macro
C
typedef int (FUNC_SX_CM_LOAD_MASK)(struct sxcmmask c, uint32_t value); #define SX_CM_LOAD_MASK ((FUNC_SX_CM_LOAD_MASK)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_CM_LOAD_MASK)))
Counter-measures are available for the AES, if enabled in HW. This function initializes the user allocated object \p c with a new counter-measures mask load operation context and reserves the HW resource.
After the initialization of \p c, this function starts the load of the counter-measure cryptographically secure random \p value. The function will return immediately. No data will be received for the load operation.
The operation is considered successful if the status returned by SX_CM_LOAD_MASK_WAIT() or SX_CM_LOAD_MASK_STATUS() is ::SX_OK.
Parameters
c counter-measures mask load operation context
Parameters
value counter-measures random value to be loaded @return ::SX_OK @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @remark | it is under the user responsibility to call it after system boot (not automatically called). | | @remark | for more details see the technical report: "Secure and Efficient | | Masking of AES | A Mission Impossible?", June 2004)
Waits until the given AES counter-measures load operation has finished.
SX_CM_LOAD_MASK_WAIT Macro
C
typedef int (FUNC_SX_CM_LOAD_MASK_WAIT)(struct sxcmmask c); #define SX_CM_LOAD_MASK_WAIT ((FUNC_SX_CM_LOAD_MASK_WAIT)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_CM_LOAD_MASK_WAIT)))
This function returns when the counter-measures load operation was successfully completed, or when an error has occurred that caused the operation to terminate.
The return value of this function is the operation status.
After this call, all resources have been released and \p c cannot be used again unless SX_CM_LOAD_MASK() is used.
Parameters
c counter-measures mask load operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_DMA_FAILED | Param | Description | |:----- |:----------- |
| @pre | SX_CM_LOAD_MASK() function must be called first @see SX_CM_LOAD_MASK_STATUS().| @remark | this function is blocking until operation finishes.
Returns the status of the given AES counter-measures load operation context.
If the operation is still ongoing, return ::SX_ERR_HW_PROCESSING. In that case, the user can retry later.
When this function returns with a code different than ::SX_ERR_HW_PROCESSING, the counter-measures mask load operation has ended and all resources used by counter-measures mask load operation context \p c have been released. In this case, \p c cannot be used for a new operation until SX_CM_LOAD_MASK() is called again.
Parameters
c counter-measures mask load operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_HW_PROCESSING @return ::SX_ERR_DMA_FAILED | Param | Description | |:----- |:----------- |
| @pre | SX_CM_LOAD_MASK() function must be called first