1.2.1.1.1.14 Common simple block cipher modes.
BLKCIPHER_API_FILE Macro
C
#define BLKCIPHER_API_FILE
All block cipher modes here perform simple encryption and decryption without any authentication.
@file @copyright Copyright (c) 2019-2020 Silex Insight. All Rights reserved.
Examples: The following examples show typical sequences of function calls for encryption and decryption of a message. @code
One-shot operation a. Encryption sx_blkcipher_create_aescbc_enc(ctx, ...) SX_BLKCIPHER_CRYPT(ctx, ...) SX_BLKCIPHER_RUN(ctx) SX_BLKCIPHER_WAIT(ctx) b. Decryption sx_blkcipher_create_aescbc_dec(ctx, ...) SX_BLKCIPHER_CRYPT(ctx, ...) SX_BLKCIPHER_RUN(ctx) SX_BLKCIPHER_WAIT(ctx)
Context-saving operation a. Encryption First round: sx_blkcipher_create_aescbc_enc(ctx) SX_BLKCIPHER_CRYPT(ctx, 'first chunk') sx_blkcipher_save_state(ctx) SX_BLKCIPHER_WAIT(ctx) Intermediary rounds: sx_blkcipher_resume_state(ctx) SX_BLKCIPHER_CRYPT(ctx, 'n-th chunk') sx_blkcipher_save_state(ctx) SX_BLKCIPHER_WAIT(ctx) Last round: sx_blkcipher_resume_state(ctx) SX_BLKCIPHER_CRYPT(ctx, 'last chunk') SX_BLKCIPHER_RUN(ctx) SX_BLKCIPHER_WAIT(ctx) b. Decryption First round: sx_blkcipher_create_aescbc_dec(ctx) SX_BLKCIPHER_CRYPT(ctx, 'first chunk') sx_blkcipher_save_state(ctx) SX_BLKCIPHER_WAIT(ctx) Intermediary rounds: sx_blkcipher_resume_state(ctx) SX_BLKCIPHER_CRYPT(ctx, 'n-th chunk') sx_blkcipher_save_state(ctx) SX_BLKCIPHER_WAIT(ctx) Last round: sx_blkcipher_resume_state(ctx) SX_BLKCIPHER_CRYPT(ctx, 'last chunk') SX_BLKCIPHER_RUN(ctx) SX_BLKCIPHER_WAIT(ctx) @endcode
Prepares an AES XTS block cipher encryption.
SX_BLKCIPHER_CREATE_AESXTS_ENC Macro
C
typedef int (FUNC_SX_BLKCIPHER_CREATE_AESXTS_ENC)(struct sxblkcipher c, const struct sxkeyref key1, const struct sxkeyref key2, const char iv); #define SX_BLKCIPHER_CREATE_AESXTS_ENC ((FUNC_SX_BLKCIPHER_CREATE_AESXTS_ENC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_CREATE_AESXTS_ENC)))
This function initializes the user allocated object \p c with a new block cipher operation context needed to run the AES XTS encryption and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the block cipher functions.
Parameters
c block cipher operation context
Parameters
key1 first key used for the block cipher operation. expected size 16, 24 or 32 bytes, must be equal to \p key2 size
Parameters
key2 second key used for the block cipher operation, expected size 16, 24 or 32 bytes, must be equal to \p key1 size
Parameters
iv initialization vector, size must be 16 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_HW_KEY_NOT_SUPPORTED @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key references provided by \p key1 and \p key2 must be initialized using SX_KEYREF_LOAD_MATERIAL().
Prepares an AES XTS block cipher decryption
SX_BLKCIPHER_CREATE_AESXTS_DEC Macro
C
typedef int (FUNC_SX_BLKCIPHER_CREATE_AESXTS_DEC)(struct sxblkcipher c, const struct sxkeyref key1, const struct sxkeyref key2, const char iv); #define SX_BLKCIPHER_CREATE_AESXTS_DEC ((FUNC_SX_BLKCIPHER_CREATE_AESXTS_DEC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_CREATE_AESXTS_DEC)))
This function initializes the user allocated object \p c with a new block cipher operation context needed to run the AES XTS decryption and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the block cipher functions.
Parameters
c block cipher operation context
Parameters
key1 first key used for the block cipher operation. expected size 16, 24 or 32 bytes, must be equal to \p key2 size
Parameters
key2 second key used for the block cipher operation, expected size 16, 24 or 32 bytes, must be equal to \p key1 size
Parameters
iv initialization vector, size must be 16 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_HW_KEY_NOT_SUPPORTED @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key references provided by \p key1 and \p key2 must be initialized using SX_KEYREF_LOAD_MATERIAL().
Prepares an AES CTR block cipher encryption.
SX_BLKCIPHER_CREATE_AESCTR_ENC Macro
C
typedef int (FUNC_SX_BLKCIPHER_CREATE_AESCTR_ENC)(struct sxblkcipher c, const struct sxkeyref key, const char iv); #define SX_BLKCIPHER_CREATE_AESCTR_ENC ((FUNC_SX_BLKCIPHER_CREATE_AESCTR_ENC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_CREATE_AESCTR_ENC)))
This function initializes the user allocated object \p c with a new block cipher operation context needed to run the AES CTR encryption and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the block cipher functions.
Parameters
c block cipher operation context
Parameters
key key used for the block cipher operation, expected size 16, 24 or 32 bytes
Parameters
iv initialization vector, size must be 16 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()
Prepares an AES CTR block cipher decryption
SX_BLKCIPHER_CREATE_AESCTR_DEC Macro
C
typedef int (FUNC_SX_BLKCIPHER_CREATE_AESCTR_DEC)(struct sxblkcipher c, const struct sxkeyref key, const char iv); #define SX_BLKCIPHER_CREATE_AESCTR_DEC ((FUNC_SX_BLKCIPHER_CREATE_AESCTR_DEC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_CREATE_AESCTR_DEC)))
This function initializes the user allocated object \p c with a new block cipher operation context needed to run the AES CTR decryption and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the block cipher functions.
Parameters
c block cipher operation context
Parameters
key key used for the block cipher operation, expected size 16, 24 or 32 bytes
Parameters
iv initialization vector, size must be 16 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()
Prepares an AES ECB block cipher encryption.
SX_BLKCIPHER_CREATE_AESECB_ENC Macro
C
typedef int (FUNC_SX_BLKCIPHER_CREATE_AESECB_ENC)(struct sxblkcipher c, const struct sxkeyref key); #define SX_BLKCIPHER_CREATE_AESECB_ENC ((FUNC_SX_BLKCIPHER_CREATE_AESECB_ENC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_CREATE_AESECB_ENC)))
This function initializes the user allocated object \p c with a new block cipher operation context needed to run the AES ECB encryption and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the block cipher functions.
Parameters
c block cipher operation context
Parameters
key key used for the block cipher operation, expected size is 16, 24 or 32 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()| @remark | AES ECB does not support context saving.
Prepares an AES ECB block cipher decryption
SX_BLKCIPHER_CREATE_AESECB_DEC Macro
C
typedef int (FUNC_SX_BLKCIPHER_CREATE_AESECB_DEC)(struct sxblkcipher c, const struct sxkeyref key); #define SX_BLKCIPHER_CREATE_AESECB_DEC ((FUNC_SX_BLKCIPHER_CREATE_AESECB_DEC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_CREATE_AESECB_DEC)))
This function initializes the user allocated object \p c with a new block cipher operation context needed to run the AES ECB decryption and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the block cipher functions.
Parameters
c block cipher operation context
Parameters
key key used for the block cipher operation, expected size 16, 24 or 32 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()| @remark | AES ECB does not support context saving.
Prepares an AES CBC block cipher encryption.
SX_BLKCIPHER_CREATE_AESCBC_ENC Macro
C
typedef int (FUNC_SX_BLKCIPHER_CREATE_AESCBC_ENC)(struct sxblkcipher c, const struct sxkeyref key, const char iv); #define SX_BLKCIPHER_CREATE_AESCBC_ENC ((FUNC_SX_BLKCIPHER_CREATE_AESCBC_ENC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_CREATE_AESCBC_ENC)))
This function initializes the user allocated object \p c with a new block cipher operation context needed to run the AES CBC encryption and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the block cipher functions.
Parameters
c block cipher operation context
Parameters
key key used for the block cipher operation, expected size 16, 24 or 32 bytes
Parameters
iv initialization vector, size must be 16 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()
Prepares an AES CBC block cipher decryption
SX_BLKCIPHER_CREATE_AESCBC_DEC Macro
C
typedef int (FUNC_SX_BLKCIPHER_CREATE_AESCBC_DEC)(struct sxblkcipher c, const struct sxkeyref key, const char iv); #define SX_BLKCIPHER_CREATE_AESCBC_DEC ((FUNC_SX_BLKCIPHER_CREATE_AESCBC_DEC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_CREATE_AESCBC_DEC)))
This function initializes the user allocated object \p c with a new block cipher operation context needed to run the AES CBC decryption and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the block cipher functions.
Parameters
c block cipher operation context
Parameters
key key used for the block cipher operation, expected size 16, 24 or 32 bytes
Parameters
iv initialization vector, size must be 16 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()
Prepares an AES CFB block cipher encryption.
SX_BLKCIPHER_CREATE_AESCFB_ENC Macro
C
typedef int (FUNC_SX_BLKCIPHER_CREATE_AESCFB_ENC)(struct sxblkcipher c, const struct sxkeyref key, const char iv); #define SX_BLKCIPHER_CREATE_AESCFB_ENC ((FUNC_SX_BLKCIPHER_CREATE_AESCFB_ENC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_CREATE_AESCFB_ENC)))
This function initializes the user allocated object \p c with a new block cipher operation context needed to run the AES CFB encryption and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the block cipher functions.
Parameters
c block cipher operation context
Parameters
key key used for the block cipher operation, expected size 16, 24 or 32 bytes
Parameters
iv initialization vector, size must be 16 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()
Prepares an AES CFB block cipher decryption
SX_BLKCIPHER_CREATE_AESCFB_DEC Macro
C
typedef int (FUNC_SX_BLKCIPHER_CREATE_AESCFB_DEC)(struct sxblkcipher c, const struct sxkeyref key, const char iv); #define SX_BLKCIPHER_CREATE_AESCFB_DEC ((FUNC_SX_BLKCIPHER_CREATE_AESCFB_DEC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_CREATE_AESCFB_DEC)))
This function initializes the user allocated object \p c with a new block cipher operation context needed to run the AES CFB decryption and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the block cipher functions.
Parameters
c block cipher operation context
Parameters
key key used for the block cipher operation, expected size 16, 24 or 32 bytes
Parameters
iv initialization vector, size must be 16 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()
Prepares an AES OFB block cipher encryption.
SX_BLKCIPHER_CREATE_AESOFB_ENC Macro
C
typedef int (FUNC_SX_BLKCIPHER_CREATE_AESOFB_ENC)(struct sxblkcipher c, const struct sxkeyref key, const char iv); #define SX_BLKCIPHER_CREATE_AESOFB_ENC ((FUNC_SX_BLKCIPHER_CREATE_AESOFB_ENC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_CREATE_AESOFB_ENC)))
This function initializes the user allocated object \p c with a new block cipher operation context needed to run the AES OFB encryption and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the block cipher functions.
Parameters
c block cipher operation context
Parameters
key key used for the block cipher operation, expected size 16, 24 or 32 bytes
Parameters
iv initialization vector, size must be 16 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()
Prepares an AES OFB block cipher decryption
SX_BLKCIPHER_CREATE_AESOFB_DEC Macro
C
typedef int (FUNC_SX_BLKCIPHER_CREATE_AESOFB_DEC)(struct sxblkcipher c, const struct sxkeyref key, const char iv); #define SX_BLKCIPHER_CREATE_AESOFB_DEC ((FUNC_SX_BLKCIPHER_CREATE_AESOFB_DEC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_CREATE_AESOFB_DEC)))
This function initializes the user allocated object \p c with a new block cipher operation context needed to run the AES OFB decryption and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the block cipher functions.
Parameters
c block cipher operation context
Parameters
key key used for the block cipher operation, expected size 16, 24 or 32 bytes
Parameters
iv initialization vector, size must be 16 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()
Adds data to be encrypted/decrypted.
SX_BLKCIPHER_CRYPT Macro
C
typedef int (FUNC_SX_BLKCIPHER_CRYPT)(struct sxblkcipher c, const char datain, size_t sz, char dataout); #define SX_BLKCIPHER_CRYPT ((FUNC_SX_BLKCIPHER_CRYPT)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_CRYPT)))
The function will return immediately.
In order to start the operation SX_BLKCIPHER_RUN() must be called.
\p sz must ensure the following restrictions based on the mode used: ##Remarks
Algorithm | \p sz | --------: | :----------: | :----------- ECB | N 16 bytes | N > 0 CBC | N 16 bytes | N > 0 CFB | N 16 bytes | N > 0 OFB | N 16 bytes | N > 0 XTS | >= 16 bytes | none CTR | > 0 bytes | none The restrictions above are applicable ONLY for the last chunk of the data to be processed when doing a partial operation. \p sz must be a multiple of block size(16 bytes) when doing a partial operation(besides last chunk).
Parameters
c block cipher operation context
Parameters
datain data to be encrypted or decrypted, with size \p sz
Parameters
sz size, in bytes, of data to be decrypted
Parameters
dataout encrypted or decrypted data, must have \p sz bytes @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_TOO_BIG | Param | Description | |:----- |:----------- |
| @pre | one of the sx_blkcipher_create_() functions must be called first
Starts a block cipher operation.
SX_BLKCIPHER_RUN Macro
C
typedef int (FUNC_SX_BLKCIPHER_RUN)(struct sxblkcipher c); #define SX_BLKCIPHER_RUN ((FUNC_SX_BLKCIPHER_RUN)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_RUN)))
This function is used to start an encryption or a decryption based on what create function was used, sx_blkcipher_create__enc() or sx_blkcipher_create__dec(). The function will return immediately.
The result will be transfered only after the operation is successfully completed. The user shall check operation status with sx_blkcipher_status() or SX_BLKCIPHER_WAIT().
Parameters
c block cipher operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_TOO_SMALL @return ::SX_ERR_WRONG_SIZE_GRANULARITY | Param | Description | |:----- |:----------- |
| @pre | SX_BLKCIPHER_CRYPT() function must be called first
Resumes AES operation in context-saving.
SX_BLKCIPHER_RESUME_STATE Macro
C
typedef int (FUNC_SX_BLKCIPHER_RESUME_STATE)(struct sxblkcipher c); #define SX_BLKCIPHER_RESUME_STATE ((FUNC_SX_BLKCIPHER_RESUME_STATE)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_RESUME_STATE)))
This function shall be called when using context-saving to load the state that was previously saved by sx_blkcipher_save_state() in the sxblkcipher operation context \p c. It must be called with the same sxblkcipher operation context \p c that was used with sx_sxblkcipher_save_state(). It will reserve all hardware resources required to run the partial AES operation. Previously used mode and direction are already stored in sxblkcipher \p c.
After successful execution of this function, the context \p c can be passed to any of the block cipher functions, except the sx_blkcipher_create_() functions.
Parameters
c block cipher operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_CONTEXT_SAVING_NOT_SUPPORTED @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | sx_blkcipher_create_aes() and sx_blkcipher_save_state() functions must be called before, for first part of the message. | | @pre | must be called for each part of the message(besides first), before sx_blkchiper_crypt() or sx_blkcipher_save_state().| @remark | the user must not change the key until all parts of the message to be encrypted/decrypted are processed. | | @remark | AES ECB does not support context saving.
Starts a partial block cipher operation.
SX_BLKCIPHER_SAVE_STATE Macro
C
typedef int (FUNC_SX_BLKCIPHER_SAVE_STATE)(struct sxblkcipher c); #define SX_BLKCIPHER_SAVE_STATE ((FUNC_SX_BLKCIPHER_SAVE_STATE)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_SAVE_STATE)))
This function is used to start a partial encryption or decryption of \p datain. The function will return immediately.
The partial result will be transfered to \p dataout only after the operation is successfully completed. The user shall check operation status with sx_blkcipher_status() or SX_BLKCIPHER_WAIT().
Parameters
c block cipher operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_CONTEXT_SAVING_NOT_SUPPORTED | Param | Description | |:----- |:----------- |
| @pre | SX_BLKCIPHER_CRYPT() should be called first.| @remark | the user must not change the key until all parts of the message to be encrypted/decrypted are processed.
Waits until the given block cipher operation has finished
SX_BLKCIPHER_WAIT Macro
C
typedef int (FUNC_SX_BLKCIPHER_WAIT)(struct sxblkcipher c); #define SX_BLKCIPHER_WAIT ((FUNC_SX_BLKCIPHER_WAIT)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_BLKCIPHER_WAIT)))
This function returns when the block cipher operation was successfully completed, or when an error has occurred that caused the operation to terminate. The return value of this function is the operation status.
After this call, all resources have been released and \p c cannot be used again unless sx_blkcipher_create_() is used.
Parameters
c block cipher operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_DMA_FAILED @see sx_blkcipher_status(). | Param | Description | |:----- |:----------- |
| @remark | this function is blocking until operation finishes.
Returns the block cipher operation status.
If the operation is still ongoing, return ::SX_ERR_HW_PROCESSING. In that case, the user can retry later.
When this function returns with a code different than ::SX_ERR_HW_PROCESSING, the block cipher operation has ended and all resources used by block cipher operation context \p c have been released. In this case, \p c cannot be used for a new operation until one of the sx_blkcipher_create_() functions is called again.
Parameters
c block cipher operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_HW_PROCESSING @return ::SX_ERR_DMA_FAILED | Param | Description | |:----- |:----------- |
| @pre | SX_BLKCIPHER_CRYPT and SX_BLKCIPHER_RUN() functions must be called first