1.2.1.1.1.4 Cryptographic message hashing SHA-2.
SXSYMCRYPT_SHA2_API_FILE Macro
C
#define SXSYMCRYPT_SHA2_API_FILE
@file
@copyright Copyright (c) 2019-2020 Silex Insight. All Rights reserved.
Hash algorithm SHA-2 224
SXHASHALG_SHA2_224 Macro
C
#define SXHASHALG_SHA2_224 ((const struct sxhashalg )((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SXHASHALG_SHA2_224)))
Has only 32 bit capacity against length extension attacks.
Hash algorithm SHA-2 256
SXHASHALG_SHA2_256 Macro
C
#define SXHASHALG_SHA2_256 ((const struct sxhashalg )((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SXHASHALG_SHA2_256)))
Has no resistance against length extension attacks.
Hash algorithm SHA-2 384
SXHASHALG_SHA2_384 Macro
C
#define SXHASHALG_SHA2_384 ((const struct sxhashalg )((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SXHASHALG_SHA2_384)))
Has 128 bit capacity against length extension attacks.
Hash algorithm SHA-2 512
SXHASHALG_SHA2_512 Macro
C
#define SXHASHALG_SHA2_512 ((const struct sxhashalg )((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SXHASHALG_SHA2_512)))
Has no resistance against length extension attacks.
Prepares a SHA256 hash operation context
SX_HASH_CREATE_SHA256 Macro
C
typedef int (FUNC_SX_HASH_CREATE_SHA256)(struct sxhash c, size_t csz); #define SX_HASH_CREATE_SHA256 ((FUNC_SX_HASH_CREATE_SHA256)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_HASH_CREATE_SHA256)))
This function initializes the user allocated object \p c with a new hash operation context and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the hashing functions.
Parameters
c hash operation context
Parameters
csz size of the hash operation context @return ::SX_OK @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @remark | SHA256 digest size is 32 bytes
Prepares a SHA384 hash operation context
SX_HASH_CREATE_SHA384 Macro
C
typedef int (FUNC_SX_HASH_CREATE_SHA384)(struct sxhash c, size_t csz); #define SX_HASH_CREATE_SHA384 ((FUNC_SX_HASH_CREATE_SHA384)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_HASH_CREATE_SHA384)))
This function initializes the user allocated object \p c with a new hash operation context and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the hashing functions.
Parameters
c hash operation context
Parameters
csz size of the hash operation context @return ::SX_OK @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @remark | SHA384 digest size is 48 bytes
Prepares a SHA512 hash operation context
SX_HASH_CREATE_SHA512 Macro
C
typedef int (FUNC_SX_HASH_CREATE_SHA512)(struct sxhash c, size_t csz); #define SX_HASH_CREATE_SHA512 ((FUNC_SX_HASH_CREATE_SHA512)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_HASH_CREATE_SHA512)))
This function initializes the user allocated object \p c with a new hash operation context and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the hashing functions.
Parameters
c hash operation context
Parameters
csz size of the hash operation context @return ::SX_OK @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @remark | SHA512 digest size is 64 bytes
Prepares a SHA224 hash operation context
This function initializes the user allocated object \p c with a new hash operation context and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the hashing functions.
Parameters
c hash operation context
Parameters
csz size of the hash operation context @return ::SX_OK @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @remark | SHA224 digest size is 28 bytes