1.2.1.1.1.15 Authenticated encryption with associated data(AEAD).
AEAD_API_FILE Macro
C
#define AEAD_API_FILE
@file @copyright Copyright (c) 2019-2020 Silex Insight. All Rights reserved.
Examples: The following examples show typical sequences of function calls for encryption and decryption a message. @code
One-shot operation a. Encryption SX_AEAD_CREATE_AESGCM_ENC(ctx, ...) SX_AEAD_FEED_AAD(ctx, aad, aadsz) SX_AEAD_CRYPT(ctx, datain, datainz, dataout) SX_AEAD_PRODUCE_TAG(ctx, tag) SX_AEAD_WAIT(ctx) b. Decryption SX_AEAD_CREATE_AESGCM_DEC(ctx, ...) SX_AEAD_FEED_AAD(ctx, aad, aadsz) SX_AEAD_CRYPT(ctx, datain, datainz, dataout) SX_AEAD_VERIFY_TAG(ctx, tag) SX_AEAD_WAIT(ctx)
Context-saving operation a. Encryption First round: SX_AEAD_CREATE_AESGCM_ENC(ctx) SX_AEAD_FEED_AAD(ctx, aad, aadsz) SX_AEAD_CRYPT(ctx, 'first chunk') SX_AEAD_SAVE_STATE(ctx) SX_AEAD_WAIT(ctx) Intermediary rounds: SX_AEAD_RESUME_STATE(ctx) SX_AEAD_CRYPT(ctx, 'n-th chunk') SX_AEAD_SAVE_STATE(ctx) SX_AEAD_WAIT(ctx) Last round: SX_AEAD_RESUME_STATE(ctx) SX_AEAD_CRYPT(ctx, 'last chunk') SX_AEAD_PRODUCE_TAG(ctx, tag) SX_AEAD_WAIT(ctx) b. Decryption First round: SX_AEAD_CREATE_AESGCM_DEC(ctx) SX_AEAD_FEED_AAD(ctx, aad, aadsz) SX_AEAD_CRYPT(ctx, 'first chunk') SX_AEAD_SAVE_STATE(ctx) SX_AEAD_WAIT(ctx) Intermediary rounds: SX_AEAD_RESUME_STATE(ctx) SX_AEAD_CRYPT(ctx, 'n-th chunk') SX_AEAD_SAVE_STATE(ctx) SX_AEAD_WAIT(ctx) Last round: SX_AEAD_RESUME_STATE(ctx) SX_AEAD_CRYPT(ctx, 'last chunk') SX_AEAD_VERIFY_TAG(ctx, tag) SX_AEAD_WAIT(ctx) @endcode
Initialization vector (IV) size, in bytes, for GCM encryption/decryption */
Size, in bytes, of GCM authentication tag */
SX_GCM_TAG_SZ Macro
C
#define SX_GCM_TAG_SZ 16u
Maximum size, in bytes, of CCM authentication tag */
Prepares an AES GCM AEAD encryption operation.
SX_AEAD_CREATE_AESGCM_ENC Macro
C
typedef int (FUNC_SX_AEAD_CREATE_AESGCM_ENC)(struct sxaead c, const struct sxkeyref key, const char iv); #define SX_AEAD_CREATE_AESGCM_ENC ((FUNC_SX_AEAD_CREATE_AESGCM_ENC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_AEAD_CREATE_AESGCM_ENC)))
This function initializes the user allocated object \p c with a new AEAD encryption operation context needed to run the AES GCM operation and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the AEAD functions.
Parameters
c AEAD operation context
Parameters
key key used for the AEAD operation, expected size 16, 24 or 32 bytes
Parameters
iv initialization vector, size must be 12 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()| @remark | \p key and \p iv buffers should not be changed until the operation is completed. | | @remark | GMAC is supported by using GCM with plaintext with size 0. | | @remark | GCM and GMAC support AAD split in multiple chunks, using context saving.
Prepares an AES GCM AEAD decryption operation.
SX_AEAD_CREATE_AESGCM_DEC Macro
C
typedef int (FUNC_SX_AEAD_CREATE_AESGCM_DEC)(struct sxaead c, const struct sxkeyref key, const char iv); #define SX_AEAD_CREATE_AESGCM_DEC ((FUNC_SX_AEAD_CREATE_AESGCM_DEC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_AEAD_CREATE_AESGCM_DEC)))
This function initializes the user allocated object \p c with a new AEAD decryption operation context needed to run the AES GCM operation and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the AEAD functions.
Parameters
c AEAD operation context
Parameters
key key used for the AEAD operation, expected size 16, 24 or 32 bytes
Parameters
iv initialization vector, size must be 12 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()| @remark | \p key and \p iv buffers should not be changed until the operation is completed. | | @remark | GMAC is supported by using GCM with ciphertext with size 0. | | @remark | GCM and GMAC support AAD split in multiple chunks, using context saving.
Prepares an AES CCM AEAD encryption operation.
SX_AEAD_CREATE_AESCCM_ENC Macro
C
typedef int (FUNC_SX_AEAD_CREATE_AESCCM_ENC)(struct sxaead c, const struct sxkeyref key, const char nonce, size_t noncesz, size_t tagsz, size_t aadsz, size_t datasz); #define SX_AEAD_CREATE_AESCCM_ENC ((FUNC_SX_AEAD_CREATE_AESCCM_ENC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_AEAD_CREATE_AESCCM_ENC)))
This function initializes the user allocated object \p c with a new AEAD encryption operation context needed to run the AES GCM operation and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the AEAD functions.
Parameters
c AEAD operation context
Parameters
key key used for the AEAD operation, expected size 16, 24 or 32 bytes
Parameters
noncesz size, in bytes, of the nonce, between 7 and 13 bytes
Parameters
nonce nonce used for the AEAD operation, with size \p noncesz
Parameters
tagsz size, in bytes, of the tag used for the AEAD operation, must be a value in {4, 6, 8, 10, 12, 14, 16}
Parameters
aadsz size, in bytes, of the additional authenticated data(AAD)
Parameters
datasz size, in bytes, of the data to be processed @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()| @remark | the same aadsz and datasz must be provided to sx_aead_encrypt() or sx_aead_decrypt() functions. | | @remark | \p key and \p nonce buffers should not be changed until the operation is completed. | | @remark | CCM DOES NOT support AAD split in multiple chunks
Prepares an AES CCM AEAD decryption operation.
SX_AEAD_CREATE_AESCCM_DEC Macro
C
typedef int (FUNC_SX_AEAD_CREATE_AESCCM_DEC)(struct sxaead c, const struct sxkeyref key, const char nonce, size_t noncesz, size_t tagsz, size_t aadsz, size_t datasz); #define SX_AEAD_CREATE_AESCCM_DEC ((FUNC_SX_AEAD_CREATE_AESCCM_DEC)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_AEAD_CREATE_AESCCM_DEC)))
This function initializes the user allocated object \p c with a new AEAD decryption operation context needed to run the AES GCM operation and reserves the HW resource.
After successful execution of this function, the context \p c can be passed to any of the AEAD functions.
Parameters
c AEAD operation context
Parameters
key key used for the AEAD operation, expected size 16, 24 or 32 bytes
Parameters
noncesz size, in bytes, of the nonce, between 7 and 13 bytes
Parameters
nonce nonce used for the AEAD operation, with size \p noncesz
Parameters
tagsz size, in bytes, of the tag used for the AEAD operation, must be a value in {4, 6, 8, 10, 12, 14, 16}
Parameters
aadsz size, in bytes, of the additional authenticated data(AAD)
Parameters
datasz size, in bytes, of the data to be processed @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()| @remark | the same aadsz and datasz must be provided to sx_aead_encrypt() or sx_aead_decrypt() functions. | | @remark | \p key and \p nonce buffers should not be changed until the operation is completed. | | @remark | CCM DOES NOT support AAD split in multiple chunks
Adds AAD chunks
SX_AEAD_FEED_AAD Macro
C
typedef int (FUNC_SX_AEAD_FEED_AAD)(struct sxaead c, const char aad, size_t aadsz); #define SX_AEAD_FEED_AAD ((FUNC_SX_AEAD_FEED_AAD)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_AEAD_FEED_AAD)))
This function is used for adding AAD buffer given by \p aad. The function will return immediately.
Parameters
c AEAD operation context
Parameters
aad additional authentication data(AAD), with size \p aadsz
Parameters
aadsz size, in bytes, of the additional authenticated data(AAD), can be 0 if \p aad is empty @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_TOO_BIG | Param | Description | |:----- |:----------- |
| @pre | one of the sx_aead_create_() functions must be called first| @remark | the additional authentication data can be empty(\p aadsz = 0) | | @remark | \p aad buffer should not be changed until the operation is completed.
Adds data to be encrypted or decrypted.
SX_AEAD_CRYPT Macro
C
typedef int (FUNC_SX_AEAD_CRYPT)(struct sxaead c, const char datain, size_t datainsz, char dataout); #define SX_AEAD_CRYPT ((FUNC_SX_AEAD_CRYPT)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_AEAD_CRYPT)))
This function is used for adding data to be processed. The function will return immediately.
The result of the operation will be transfered to \p dataout after the operation is successfully completed.
For context saving, \p datain size(\p datainsz) must be a multiple of 16 bytes for AES GCM and CCM and a multiple of 64 bytes for ChaCha20Poly1305, except the last buffer.
Parameters
c AEAD operation context
Parameters
datain data to be encrypted or decryoted, with size \p datainsz
Parameters
datainsz size, in bytes, of the data to be encrypted or decrypted
Parameters
dataout encrypted or decrypted data, must have \p datainsz bytes @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_TOO_BIG | Param | Description | |:----- |:----------- |
| @pre | one of the sx_aead_create_() functions must be called first| @remark | \p datain buffer should not be changed until the operation is completed.
Starts an AEAD encryption and tag computation.
SX_AEAD_PRODUCE_TAG Macro
C
typedef int (FUNC_SX_AEAD_PRODUCE_TAG)(struct sxaead c, char tagout); #define SX_AEAD_PRODUCE_TAG ((FUNC_SX_AEAD_PRODUCE_TAG)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_AEAD_PRODUCE_TAG)))
The function will return immediately.
The computed tag will be transfered to \p tag only after the operation is successfully completed.
The user shall check operation status with sx_aead_status() or SX_AEAD_WAIT().
Parameters
c AEAD operation context
Parameters
tag authentication tag @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_TOO_BIG | Param | Description | |:----- |:----------- |
| @pre | one of the SX_AEAD_FEED_AAD() or SX_AEAD_CRYPT() functions must be called first| @remark | if used with context saving(last chunk), the fed data size for the last chunk can not be 0
Starts an AEAD decryption and tag validation.
SX_AEAD_VERIFY_TAG Macro
C
typedef int (FUNC_SX_AEAD_VERIFY_TAG)(struct sxaead c, const char tagin); #define SX_AEAD_VERIFY_TAG ((FUNC_SX_AEAD_VERIFY_TAG)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_AEAD_VERIFY_TAG)))
The function will return immediately.
The user shall check operation status with sx_aead_status() or SX_AEAD_WAIT().
Parameters
c AEAD operation context
Parameters
tag authentication tag @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_TOO_BIG | Param | Description | |:----- |:----------- |
| @pre | one of the SX_AEAD_FEED_AAD() or SX_AEAD_CRYPT() functions must be called first| @remark | \p tag buffer should not be changed until the operation is completed. | | @remark | if used with context saving(last chunk), the fed data size for the last chunk can not be 0
Resumes AEAD operation in context-saving.
SX_AEAD_RESUME_STATE Macro
C
typedef int (FUNC_SX_AEAD_RESUME_STATE)(struct sxaead c); #define SX_AEAD_RESUME_STATE ((FUNC_SX_AEAD_RESUME_STATE)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_AEAD_RESUME_STATE)))
This function shall be called when using context-saving to load the state that was previously saved by sx_aead_save_state() in the sxaead operation context \p c. It must be called with the same sxaead operation context \p c that was used with sx_aead_save_state(). It will reserve all hardware resources required to run the partial AEAD operation. Previously used mode and direction are already stored in sxaead \p c.
After successful execution of this function, the context \p c can be passed to any of the AEAD functions, except the sx_aead_create_() functions.
Parameters
c AEAD operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_CONTEXT_SAVING_NOT_SUPPORTED @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | sx_aead_create_aes() and sx_aead_save_state() functions must be called before, for first part of the message. | | @pre | must be called for each part of the message(besides first), before SX_AEAD_CRYPT() or sx_aead_save_state().| @remark | the user must not change the key until all parts of the message to be encrypted/decrypted are processed.
Starts a partial AEAD operation.
SX_AEAD_SAVE_STATE Macro
C
typedef int (FUNC_SX_AEAD_SAVE_STATE)(struct sxaead c); #define SX_AEAD_SAVE_STATE ((FUNC_SX_AEAD_SAVE_STATE)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_AEAD_SAVE_STATE)))
This function is used to start a partial encryption or decryption of \p datain. The function will return immediately.
The partial result will be transfered to \p dataout only after the operation is successfully completed. The user shall check operation status with sx_aead_status() or SX_AEAD_WAIT().
Parameters
c AEAD operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_CONTEXT_SAVING_NOT_SUPPORTED @return ::SX_ERR_WRONG_SIZE_GRANULARITY | Param | Description | |:----- |:----------- |
| @pre | SX_AEAD_CRYPT() should be called first.| @remark | the user must not change the key until all parts of the message to be encrypted/decrypted are processed. | | @remark | when in context saving, the sizes of the chunks fed must be multiple of 16 bytes, besides the last chunk that can be any size, but not 0
Waits until the given AEAD operation has finished
SX_AEAD_WAIT Macro
C
typedef int (FUNC_SX_AEAD_WAIT)(struct sxaead c); #define SX_AEAD_WAIT ((FUNC_SX_AEAD_WAIT)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_AEAD_WAIT)))
This function returns when the AEAD operation was successfully completed, or when an error has occurred that caused the operation to terminate.
The return value of this function is the operation status.
After this call, all resources have been released and \p c cannot be used again unless sx_aead_create_() is used.
making \p c unusable for a new operation without calling, first, one of the sx_aead_create_() functions.
Parameters
c AEAD operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_DMA_FAILED @return ::SX_ERR_INVALID_TAG | Param | Description | |:----- |:----------- |
| @pre | sx_aead_encrypt or sx_aead_decrypt() function must be called first @see sx_aead_status().| @remark | this function is blocking until operation finishes.
Returns the AEAD operation status.
If the operation is still ongoing, return ::SX_ERR_HW_PROCESSING. In that case, the user can retry later.
When this function returns with a code different than ::SX_ERR_HW_PROCESSING, the AEAD operation has ended and all resources used by the AEAD operation context \p c have been released. In this case, \p c cannot be used for a new operation until one of the sx_aead_create_() functions is called again.
Parameters
c AEAD operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_HW_PROCESSING @return ::SX_ERR_DMA_FAILED @return ::SX_ERR_INVALID_TAG | Param | Description | |:----- |:----------- |
| @pre | sx_aead_encrypt or sx_aead_decrypt() function must be called first| @remark | if authentication fails during decryption, ::SX_ERR_INVALID_TAG will be returned. In this case, the decrypted text is not valid and shall not be used.