1.2.1.1.1.11 Cryptographic message hashing.
HASH_API_FILE Macro
C
#define HASH_API_FILE
@file
@copyright Copyright (c) 2019-2020 Silex Insight. All Rights reserved.
Examples: The following examples show typical sequences of function calls for hashing a message. @code
Single-call hash computation SX_HASH_CREATE(ctx, &sxhashalg_sha2_256, ctxsize) SX_HASH_FEED(ctx, 'chunk 1') SX_HASH_FEED(ctx, 'chunk 2') SX_HASH_DIGEST(ctx) SX_HASH_WAIT(ctx)
Context-saving hash computation First round: SX_HASH_CREATE(ctx, &sxhashalg_sha2_256, ctxsize) SX_HASH_FEED(ctx, 'chunk 1 of first round') SX_HASH_FEED(ctx, 'chunk 2 of first round') SX_HASH_SAVE_STATE(ctx) SX_HASH_WAIT(ctx) Intermediary rounds: SX_HASH_RESUME_STATE(ctx) SX_HASH_FEED(ctx, 'chunk 1 of round i') SX_HASH_FEED(ctx, 'chunk 2 of round i') SX_HASH_FEED(ctx, 'chunk 3 of round i') SX_HASH_SAVE_STATE(ctx) SX_HASH_WAIT(ctx) Last round: SX_HASH_RESUME_STATE(ctx) SX_HASH_FEED(ctx, 'chunk 1 of last round') SX_HASH_FEED(ctx, 'chunk 2 of last round') SX_HASH_DIGEST(ctx) SX_HASH_WAIT(ctx) @endcode
Creates a hash operation context
SX_HASH_CREATE Macro
C
typedef int (FUNC_SX_HASH_CREATE)(struct sxhash c, const struct sxhashalg alg, size_t csz); #define SX_HASH_CREATE ((FUNC_SX_HASH_CREATE)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_HASH_CREATE)))
This function initializes the user allocated object \p c with a new hash operation context and reserves the HW resource. After successful execution of this function, the context \p c can be passed to any of the hashing functions.
Parameters
c hash operation context
Parameters
alg hash algorithm
Parameters
csz size of the hash operation context @return ::SX_OK @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY
Return the digest size produced by the given hash algorithm */
Return the block size used by the given hash algorithm */
SX_HASH_GET_ALG_BLOCKSZ Macro
C
typedef size_t (FUNC_SX_HASH_GET_ALG_BLOCKSZ)(const struct sxhashalg alg); #define SX_HASH_GET_ALG_BLOCKSZ ((FUNC_SX_HASH_GET_ALG_BLOCKSZ)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_HASH_GET_ALG_BLOCKSZ)))
Resume hashing in context-saving (partial hashing).
SX_HASH_RESUME_STATE Macro
C
typedef int (FUNC_SX_HASH_RESUME_STATE)(struct sxhash c); #define SX_HASH_RESUME_STATE ((FUNC_SX_HASH_RESUME_STATE)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_HASH_RESUME_STATE)))
This function shall be called when using context-saving to load the state that was previously saved by SX_HASH_SAVE_STATE() in the sxhash operation context \p c. It must be called with the same sxhash operation context \p c that was used with SX_HASH_SAVE_STATE(). It will reserve all hardware resources required to run the partial hashing.
Parameters
c hash operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ | Param | Description | |:----- |:----------- |
| @pre | SX_HASH_SAVE_STATE() function must be called before | | @pre | must be called before SX_HASH_FEED() for the next partial message
Assign data to be hashed.
SX_HASH_FEED Macro
C
typedef int (FUNC_SX_HASH_FEED)(struct sxhash c, const char chunk, size_t sz); #define SX_HASH_FEED ((FUNC_SX_HASH_FEED)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_HASH_FEED)))
This function adds a chunk of data to be hashed. It can be called multiple times to assemble pieces of the message scattered in memory.
In context-saving, the sum of the sizes of the chunks fed must be multiple of the block size of the algorithm used. If this condition is not met before calling SX_HASH_SAVE_STATE(), SX_HASH_SAVE_STATE() will return ::SX_ERR_WRONG_SIZE_GRANULARITY
Parameters
c hash operation context
Parameters
msg message to be hashed
Parameters
sz size in bytes of \p msg, maximum value is 2^24-1 bytes @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_FEED_COUNT_EXCEEDED @return ::SX_ERR_TOO_BIG | Param | Description | |:----- |:----------- |
| @pre | one of the SX_HASH_CREATE_() functions must be called first | | @pre | if in context-saving, SX_HASH_RESUME_STATE() must be called first| @remark | if return value is ::SX_ERR_FEED_COUNT_EXCEEDED or ::SX_ERR_TOO_BIG, \p c cannot be used anymore. | | @remark | if this function is called with \p sz equal to 0, no data will be assigned to be hashed, ::SX_OK will be returned. | | @remark | default maximum number of feeds for single-call digest is 6 and for context-saving is 4. | | @remark | maximum sum of the chunk sizes fed is 2^32-1 bytes
Starts the partial hashing operation.
SX_HASH_SAVE_STATE Macro
C
typedef int (FUNC_SX_HASH_SAVE_STATE)(struct sxhash c); #define SX_HASH_SAVE_STATE ((FUNC_SX_HASH_SAVE_STATE)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_HASH_SAVE_STATE)))
This function updates the partial hashing based on the data chunks fed since the last call to SX_HASH_RESUME_STATE().
In order to export the state of partial hashing, the total size of data fed in the current resume-save step must be multiple of block size of the algorithm used. For SHA1/224/256/SM3 block size is 64 bytes and for SHA384/512 block size is 128 bytes.
The function will return immediately. The hash state will be saved in the sxhash structure after the operation successfully completed. The user shall check operation status with SX_HASH_STATUS() or SX_HASH_WAIT().
Parameters
c hash operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_WRONG_SIZE_GRANULARITY | Param | Description | |:----- |:----------- |
| @pre | one of the SX_HASH_CREATE_() functions or SX_HASH_RESUME_STATE() must be called first| @remark | if return value is ::SX_ERR_WRONG_SIZE_GRANULARITY, \p c cannot be used anymore. | | @remark | the content of the input data buffers, provided with previous calls to SX_HASH_FEED(), should not be changed until the operation is completed. Checking the completion of an operation is done by using SX_HASH_WAIT() or SX_HASH_STATUS().
Starts the hashing operation.
SX_HASH_DIGEST Macro
C
typedef int ( FUNC_SX_HASH_DIGEST)(struct sxhash c, char digest); #define SX_HASH_DIGEST ((FUNC_SX_HASH_DIGEST)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_HASH_DIGEST)))
This function is used to start the computation of the digest. If used in context-saving approach, this function will compute the digest based on last computed state and last chunks of the message.
The function will return immediately. The result will be transfered to \p digest only after the operation is successfully completed. The user shall check operation status with SX_HASH_STATUS() or SX_HASH_WAIT().
Parameters
c hash operation context
Parameters
digest result of the hash operation, user must allocate enough memory for it. In order to get the amount of memory needed for the digest, the user can use SX_HASH_GET_DIGESTSZ() or check the corresponding SX_HASH_CREATE_() function. @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ | Param | Description | |:----- |:----------- |
| @pre | one of the SX_HASH_CREATE_() functions must be called first| @remark | the content of the input data buffers, provided with previous calls to SX_HASH_FEED(), should not be changed until the operation is completed. Checking the completion of an operation is done by using SX_HASH_WAIT() or SX_HASH_STATUS().
Waits until the given hash operation has finished
SX_HASH_WAIT Macro
C
typedef int (FUNC_SX_HASH_WAIT)(struct sxhash c); #define SX_HASH_WAIT ((FUNC_SX_HASH_WAIT)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_HASH_WAIT)))
This function returns when the hash operation was successfully completed, or when an error has occurred that caused the operation to terminate.
The return value of this function is the operation status.
After this call, all resources have been released and \p c cannot be used again unless SX_HASH_CREATE_() is used.
Parameters
c hash operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_HW_PROCESSING @return ::SX_ERR_DMA_FAILED | Param | Description | |:----- |:----------- |
| @pre | SX_HASH_DIGEST() functions must be called first | | @pre | if in context-saving, SX_HASH_SAVE_STATE() must be called first @see SX_HASH_STATUS().| @remark | this function is blocking until operation finishes. | | @remark | this function calls SX_HASH_STATUS() in loop until operation is completed.
Returns the status of the given hash operation context.
SX_HASH_STATUS Macro
C
typedef int (FUNC_SX_HASH_STATUS)(struct sxhash c); #define SX_HASH_STATUS ((FUNC_SX_HASH_STATUS)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_HASH_STATUS)))
If the operation is still ongoing, return ::SX_ERR_HW_PROCESSING. In that case, the user can retry later.
When this function returns with a code different than ::SX_ERR_HW_PROCESSING, the hash operation has ended and all associated hardware resources used by hash operation context \p c have been released. If SX_HASH_DIGEST() was used, \p c cannot be used for a new operation until one of the SX_HASH_CREATE_() functions is called again. If SX_HASH_SAVE_STATE() was used, then \p c shall be reused with sx_hash_resume().
Parameters
c hash operation context @return ::SX_OK @return ::SX_ERR_UNITIALIZED_OBJ @return ::SX_ERR_HW_PROCESSING @return ::SX_ERR_DMA_FAILED | Param | Description | |:----- |:----------- |
| @pre | SX_HASH_DIGEST() functions must be called first | | @pre | if in context-saving, SX_HASH_SAVE_STATE() must be called first.
Returns digest size in bytes for the hash operation context.
SX_HASH_GET_DIGESTSZ Macro
C
typedef size_t (FUNC_SX_HASH_GET_DIGESTSZ)(struct sxhash c); #define SX_HASH_GET_DIGESTSZ ((FUNC_SX_HASH_GET_DIGESTSZ)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_HASH_GET_DIGESTSZ)))
Parameters
c hash operation context @return digest size in bytes of the algorithm specified by \p c | Param | Description | |:----- |:----------- |
| @pre | one of the SX_HASH_CREATE_() functions must be called first
Returns block size in bytes for the hash operation context.
SX_HASH_GET_BLOCKSZ Macro
C
typedef size_t (FUNC_SX_HASH_GET_BLOCKSZ)(struct sxhash c); #define SX_HASH_GET_BLOCKSZ ((FUNC_SX_HASH_GET_BLOCKSZ)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_HASH_GET_BLOCKSZ)))
Parameters
c hash operation context @return block size in bytes of the algorithm specified by \p c | Param | Description | |:----- |:----------- |
| @pre | one of the SX_HASH_CREATE_() functions must be called first
Abandon a created hash operation context.
A created hash operation context can have reserved hardware and software resources. Those are free-ed automatically on error or when the operation finishes as reported by SX_HASH_STATUS() or SX_HASH_WAIT(). If for some reason, the hash operation will not be started, it can be abandoned which will release all reserved resources.
Can only be called after a call to one of the SX_HASH_CREATE_() or after sx_hash_resume(). It must be called BEFORE starting to run the operation with SX_HASH_DIGEST() or SX_HASH_SAVE_STATE().
Parameters
c hash operation context