40.7.4 Standard Read and Write Protocols
In the following sections, the byte access type is not considered. Byte select lines (NBS0 and NBS1) always have the same timing as the address bus. NWE represents either the NEW signal in byte select access type or one of the byte write lines (NWR0 to NWR1) in byte write access type. NWR0 to NWR1 have the same timings and protocol as NWE. In the same way, NCS represents one of the NCS[0..NB_CS-1] chip select lines.