44.7.25 ADC Interrupt Flags Register

Note: Interrupt flags must be cleared and then read back to confirm they are cleared before exiting the ISR to avoid double interrupts.
Table 44-30. Register Bit Attribute Legend
SymbolDescriptionSymbolDescriptionSymbolDescription
RReadable bitHCCleared by Hardware(Grey cell)Unimplemented
WWritable bitHSSet by HardwareXBit is unknown at Reset
KWrite to clearSSoftware settable bit——
Name: INTFLAG
Offset: 0x128
Reset: 0x00000000
Property: -

Bit 3130292827262524 
 CHRDY[15:8] 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 
Bit 2322212019181716 
 CHRDY[7:0] 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 
Bit 15141312111098 
 CRDYID[3:0]EOSRDYCHNERRCFLTRDYCHRDYC 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 
Bit 76543210 
 SOVFL  CMPHITCMPINTID[3:0] 
Access R/WR/WR/WR/WR/WR/W 
Reset 000000 

Bits 31:16 – CHRDY[15:0] ADC Channel Ready Interrupt Flag Channel k

CHRDY[ k ] = 1 indicates that ADC has completed its last A/D conversion for channel k.

Note: CHRDY[ k ] = 14-0 individual channels which corresponds to VINP[14:0]. K=11 and 10 do not exist for the 64-pin package.

If INTENSET.CHRDY[ k ] is set, then CHRDY[ k ] = 1 will trigger an ADC interrupt.

CHRDY[ k ] is reset by software writing a 1 to it.

Bits 15:12 – CRDYID[3:0] ADC Module Current Channel ID Ready Bits

The value of CRDYID indicates the input channel index, k , that ADC has just completed in its current scan. This if for information only since these bits cannot be used to trigger an ADC interrupt. (CHRDY[ k ] are intended for that purpose.)

These bits are reset by software writing a 1 to them.

Bit 11 – EOSRDY ADC Module End-Of-Scan Interrupt Flag

This bit is set by hardware at the end of the scan of all channels included in the scan performed by ADC in response to a SINGLE event of the Scan Trigger 0 (STRIG0).

If INTENSET.EOSRDY is set, then EOSRDY = 1 will trigger an ADC interrupt.

This bit is reset by software writing a 1 to it.

Bit 10 – CHNERRC ADC Module Channel Overwritten Error Flag

When set, this bit indicates that the ADC has completed its last A/D conversion for channel CRDYID[3:0], but at the time CRDYID[3:0] was updated, the status bit CHRDYC was still set, which indicates that the software may not have had the time to read the previous data, which may be now lost.

If INTENSET.CHNERRC is set, then CHNERRC = 1 will trigger an ADC interrupt.

This bit is reset by software writing a 1 to it.

Bit 9 – FLTRDY ADC Digital Filter Ready for Filter Flag

When set, this bit indicates that the digital filter has issued a new output sample for the input channel defined by FLTCTRL.FLTCHNID.

If INTENSET.FLTRDY is set, then FLTRDY = 1 will trigger an ADC interrupt.

This bit is reset by software writing a 1 to it.

Bit 8 – CHRDYC ADC Current Channel Ready Flag

0 = ADC busy or idle.

1 = When set, this bit signifies that the ADC has completed its current A/D conversion for the channel identified in CRDYID[3:0].

Note:
  1. If INTENSET.CHRDYC is set, then CHRDYC = 1 will trigger an ADC interrupt.
  2. This bit is reset by software writing a 1 to it.

Bit 7 – SOVFL ADC Clock Synchronizer Overflow into the APB Clock Domain

When set this bit signifies the ADC data was lost due to a slow APB_CLK.

If INTENSET.SOVFL is set, then SOVFL = 1 will trigger an ADC interrupt.

This bit is reset by software writing a 1 to it.

Bit 4 – CMPHIT ADC Digital Comparator Hit Interrupt Flag for Comparator

When set, this bit signifies that the Digital Comparator associated with ADC has issued a condition hit interrupt for channel identified in CMPINTID[5:0].

If INTENSET.CMPHIT is set, then CMPHIT = 1 will trigger an ADC interrupt.

This bit is reset by software writing a 1 to it.

Bits 3:0 – CMPINTID[3:0] ADC Module Digital Comparator Channel ID Bits

When set, this signifies that the ADC Channel ID for which the digital comparator has issued the condition hit interrupt (CMPHIT=1). These bits cannot be used as an interrupt request flag. This is for information only. (CMPHIT is intended for that purpose.)

This bit is reset by software writing a 1 to it.