4.33.1 GVRP Port Configuration
The GVRP Port Configuration page has the following parameters:
- Port: The logical port that is to be configured.
- Mode: Can be either Disabled or GVRP enabled. These values turn the GVRP feature off or on respectively for the port in question.