4.23.1 Port to Group Configurations
The following sections describe the VLAN Translation Configurations.
The VLAN Translation Port Configuration page has the following parameters:
- Port: The Port column shows the list of ports for which you can configure the VLAN Translation Mapping Group.
- Default: To set the switch port to use the default VLAN Translation Group click the checkbox and press Save.
- Group ID: The VLAN Translation
mappings are organized into Groups, identified by the Group ID. This way a port is
configured to use a number of VLAN Translation mappings easily by simply configuring
it to use a given group. Then number of possible groups in a switch is equal to the
number of ports present in this switch. A port can be configured to use any of the
groups, but only one at any given time. Multiple ports can be configured to use the
same group. A valid Group ID is an integer value from 1-8. Note: By default, each port is set to use the group with Group ID equal to the port number. For example, port #1 is by default set to use group with GID = 1.