4.10.2.5.2 Network IPv6 Source Guard Static Table Configuration
The IPv6 Source Guard Static Table page shows the static IPv6 Source Guard entries. The maximum number of entries is 112 on the switch.

The IPv6 Source Guard Static Table page has the following parameters:
- Delete: Click entry Delete to delete the entry
- Port: The logical port to which the entry is bound
- VLAN ID: The VLAN ID for the entry. If no VLAN ID is associated with the entry, this field shows 0.
- IPv6 Address: Allowed Source IPv6 address
- Prefix Size: Prefix size of the IPv6 address
- Mac Address: Allowed Source MAC address