4.32.1 MVRP Global and Port Configuration
The MVRP Global and Port Configuration page has the following parameters:
- Global State: Enables/Disables the MVRP protocol globally, and at the same time on the switch ports that are MVRP enabled.
- Managed VLANs: This field shows the managed VLANs, that is, the VLANs that MVRP will operate upon. By default, only VLANs 1-4094 are managed, that is, the entire range as defined in IEEE802.1Q-2014 for MVRP. However this range can be limited by using a list syntax where the individual elements are separated by commas. Ranges are specified with a dash separating the lower and upper bound. The following example will create VLANs 1, 10, 11, 12, 13, 200, and 300: 1, 10-13,200,300. Spaces are allowed in between the delimiters.
- Port: The port number for which the following configuration applies.
- Enabled: Enable/Disable the MVRP protocol on this switch port, given that MVRP is also globally enabled.