5.11.2.5 Monitor-Security-Network-IP Source Guard
Each page shows up to 99 entries from the Dynamic IP Source Guard table, default being 20, selected through the entries per page input field. When first visited, the web page will show the first 20 entries from the beginning of the Dynamic IP Source Guard Table. The Start from port address, VLAN and IP address input fields allow the user to select the starting point in the Dynamic IP Source Guard Table. Clicking the Refresh button will update the displayed table starting from that or the closest next Dynamic IP Source Guard Table match. In addition, the two input fields will - upon a Refresh button click - assume the value of the first displayed entry, allowing for continuous refresh with the same start address. The >> button will use the last entry of the currently displayed table as a basis for the next lookup. When the end is reached the text No more entries is shown in the displayed table. Use the |<< button to start over.

The Dynamic IP Source Guard Table page has the following parameters:
- Port: Switch Port Number for which the entries are displayed
- VLAN ID: VLAN-ID in which the IP traffic is permitted
- IP Address: User IP address of the entry
- MAC Address: Source MAC address