5.11.2.6 Monitor-Security-Network-IPv6 Source Guard
Entries in the Dynamic IPv6 Source Guard Table are shown on the IPv6 Source Guard Dynamic Table page.

The IPv6 Source Guard Dynamic Table page has the following parameters:
- Port: Switch Port Number to which the entries are bound
- VLAN ID: VLAN-ID in which the IP traffic is permitted. If no VLAN-ID is associated with the entry, this field shows 0.
- IPv6 Address: Source IPv6 address of the entry
- MAC Address: Source MAC address