4.15.2 IPMC Profile Address Configuration

The following sections describe the IPMC Profile Address configuration parameters.
- Delete: Check to delete the entry. The designated entry will be deleted during the next save.
- Entry Name: The name used for indexing the address entry table. Each entry has the unique name which is composed of at maximum 16 alphabetic and numeric characters. At least one alphabet must be present.
- Start Address: The starting IPv4/IPv6 Multicast Group Address that will be used as an address range.
- End Address: The ending IPv4/IPv6 Multicast Group Address that will be used as an address range.