5.9.1 Monitor DHCPv4 Snooping Table
The Dynamic DHCP Snooping Table page displays the dynamic IP assigned information after DHCP Snooping mode is disabled. All DHCP clients obtained the dynamic IP address from the DHCP server are listed in this table except for local VLAN interface IP addresses. Entries in the Dynamic DHCP snooping table are shown on this page. Each page shows up to 99 entries from the Dynamic DHCP snooping table, default being 20, selected through the entries per page input field. When first visited, the web page shows the first 20 entries from the beginning of the Dynamic DHCP Snooping table. The MAC address and VLAN input fields allow you to select the starting point in the Dynamic DHCP snooping table.

The Dynamic DHCP Snooping Table page has the following parameters:
- MAC Address: User MAC address of the entry
- VLAN ID: VLAN-ID in which the DHCP traffic is permitted
- Source Port: Switch Port Number for which the entries are displayed
- IP Address: User IP address of the entry
- IP Subnet Mask: User IP subnet mask of the entry
- DHCP Server Address: DHCP Server address of the entry