5.12.4 Monitor-Aggregation-LACP-Internal Status
The LACP Internal Port Status page provides a status overview for the LACP internal (that is, the local system) status for all ports. Only ports that are part of an LACP group are shown. For details on the shown parameters, see the IEEE 801.AX-2014.

The LACP Internal Port Status page has the following parameters:
- Port: The switch port number
- State: The current port state:
- Down: The port is not active
- Active: The port is in active state
- Standby: The port is in standby state
- Key: The key assigned to this port. Only ports with the same key can aggregate together.
- Priority: The priority assigned to this aggregation group
- Activity: The LACP mode of the group (Active or Passive)
- Timeout: The timeout mode configured for the port (Fast or Slow)
- Aggregation: Shows whether the system considers this link to be aggregatable; that is, a potential candidate for aggregation.
- Synchronization: Shows whether the system considers this link to be IN_SYNC; that is, it has been allocated to the correct LAG, the group has been associated with a compatible Aggregator, and the identity of the LAG is consistent with the System ID and operational Key information transmitted.
- Collecting: Shows if collection of incoming frames on this link is enabled
- Distributing: Shows if distribution of outgoing frames on this link is enabled
- Defaulted: Shows if the Actor's Receive machine is using Defaulted operational Partner information
- Expired: Shows if that the Actor's Receive machine is in the EXPIRED state