4.17.1 IGMP Snooping Basic Configuration
This page provides IGMP Snooping related configuration.

- Snooping Enabled: Enable the Global IGMP Snooping.
- Unregistered IPMCv4 Flooding Enabled: Enable unregistered IPMCv4 traffic flooding. The flooding control takes effect only when IGMP Snooping is enabled. When IGMP Snooping is disabled, unregistered IPMCv4 traffic flooding is always active in spite of this setting.
- IGMP SSM Range: SSM (Source-Specific Multicast) Range allows the SSM-aware hosts and routers run the SSM service model for the groups in the address range. Requests made by IGMPv1 and IGMPv2 hosts in this range are ignored. Assign a valid IPv4 multicast address as prefix with a prefix length (from 4 to 32) for the range.
- Leave Proxy Enabled: Enable IGMP Leave Proxy. This feature can be used to avoid forwarding unnecessary leave messages to the router side.
- Proxy Enabled: Enable IGMP Proxy. This feature can be used to avoid forwarding unnecessary join and leave messages to the router side.
- Router Port: Specify which ports act as router ports. A router port is a port on the Ethernet switch that leads towards the Layer 3 multicast device or IGMP Querier. If an aggregation member port is selected as a router port, the whole aggregation will act as a router port.
- Fast Leave: Enable the fast leave on the port. System will remove group record and stop forwarding data upon receiving the IGMPv2 leave message without sending last member query messages. It is recommended to enable this feature only when a single IGMPv2 host is connected to the specific port.
- Throttling: Enable to limit the number of multicast groups to which a switch port can belong.